Caterpillar to Unveil Well Stimulation Pumps at OTC 2013

Houston, TX – Caterpillar Global Petroleum is pleased to announce the launch of Cat® Well Stimulation Pumps for the well service market. Starting in May 2013, Caterpillar will begin accepting orders for the Cat WS223, a 2250 bhp (1678 bkW) triplex well stimulation pump, as well as the Cat WS255, a 2500 bhp (1864 bkW) quintuplex well stimulation pump. In addition to offering the complete pump for well service customers, Caterpillar will offer a variety of 8” and 10” stroke fluid ends individually. A 2700hp triplex pump, available in late 2013, will be on display along with several fluid end models at the Caterpillar booth #3341 at OTC 2013, May 6th – 9th in Houston, Texas.

“At Caterpillar, our goal is to provide the most reliable and durable power solutions for the Well Service and Pressure Pumping market. By adding the well stimulation pumps to our portfolio of offerings we are able to provide a more comprehensive pressure pumping solution for our customers,” Mark Helgren, Caterpillar Global Petroleum integration manager stated. “Our customers, who have been pleased with our engines and transmissions, will be able to readily implement the Cat well stimulation pumps into their operations with the utmost confidence in their performance and Cat Dealer support.”

The Cat Well Stimulation Pumps feature fluid ends and power ends designed to an industry standard footprint. This will allow customers to easily fit the Cat pump into their existing trailer designs. In addition to the standard fluid end Cat will offer an Extreme Duty (XD) fluid end with superior durability for the harshest operating conditions. The fluid ends on both models have a valve-over-valve design to simplify valve, seat and plunger installation, and each fluid end block is manufactured with a robust material conditioning process. A full assortment of discharge flanges, suction manifolds, and bore sizes will also be offered.

The new Cat well stimulation pumps will be distributed, sold and supported through the worldwide Cat dealer network with trained technicians to ensure service support is never out of reach. For more information, please visit the well stimulation pump website or stop by the Caterpillar booth at OTC Houston, May 6-9, Booth #3341. For up to the minute information during OTC, follow us on Facebook: http://www.facebook.com/caterpillaroilandgas & Twitter: http://www.twitter.com/catoilandgas using #OTCHOUSTON and #CatatOTC.

# # #

About Caterpillar Global Petroleum

Caterpillar Global Petroleum, Caterpillar Inc.’s oil and gas division with headquarters in Houston, Texas, groups all the sales and service activities for Cat oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at: http://www.catoilandgasinfo.com/pr

About Caterpillar

For more than 85 years, Caterpillar Inc. has been making progress possible and driving positive and sustainable change on every continent. With 2012 sales and revenues of $65.875 billion, Caterpillar is a technology leader and the world’s leading manufacturer of construction and mining equipment, clean diesel and natural gas engines and industrial gas turbines. More information is available at www.cat.com.

Note to Editors: Caterpillar rolls-out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

Press Inquiries

Caterpillar Press Relations:

Jenna Janik
Tel: +1.713.895.1449
Janik_Jenna_E@cat.com