New Cat® M Series 3 Motor Graders Deliver Greater Fuel Efficiency, Enhanced Safety and Comfort, Easier Service and Reduced Emissions

For Release in North America: January 2014
Release Number: 530PR13

The new Cat® M Series 3 motor graders—12M3, 140M3, 160M3 and their all-wheel-drive (AWD) counterparts—bring the latest emissions reduction technology to the most durable, productive and comfortable graders on the market. The new models offer greater fuel efficiency, more operator comfort and safety features, as well as enhanced serviceability. M Series 3 motor graders meet U.S. EPA Tier 4 Final/EU Stage IV emission standards.

Fuel Efficiency and Emissions Reduction
M Series 3 motor graders meet U.S. EPA Tier 4 Final/EU Stage IV emission standards using emissions reduction technology that is designed to be transparent, with no action required by the operator. There is no need to stop for regeneration. The system uses Caterpillar’s proven aftertreatment solution with the addition of Selective Catalytic Reduction (SCR). SCR utilizes Diesel Exhaust Fluid (DEF), which can be conveniently filled from ground level when the machine is fueled. Because of improved fuel economy over Tier 4 Interim and efficient use of DEF, M Series 3 motor graders deliver excellent overall fluid efficiency.

A new standard Economy (ECO) Mode can be turned on to help save fuel by reducing engine speed so the machine works in a more efficient range. The average fuel savings is up to 10 percent, depending on the application.

Integrated Technologies
Cat Connect makes smart use of technology and services to help improve jobsite efficiency. M Series 3 motor graders are equipped with Product Link™, which helps fleet owners track location, hours, fuel usage, productivity, idle time, and diagnostic codes through the online VisionLink® interface. M Series 3 machines also offer optional grade technologies like Cat Grade Control Cross Slope and Cat AccuGrade™ help operators work more efficiently, productively and accurately.

Comfort and Convenience
In the cab, operators will find the hallmark Cat motor grader controls—two electronic joysticks that reduce arm movement by 78% to help lessen operator fatigue and enhance productivity.  M Series 3 models also feature a redesigned message display located in the center console of the machine. The display puts Cat Grade Control Cross Slope information conveniently in front of the operator, and also includes a DEF tank level gauge. Operators will also enjoy a more comfortable seat with heated and ventilated options, an optional seat belt indicator light, and several convenient new storage bins located throughout the cab. An additional convenience feature can be found in the engine compartment. New optional LED lights make it easier to service the machine in low light conditions.

For more information about Cat M Series 3 Motor Graders, contact the local Cat dealer or go to: http://www.cat.com/en_US/products/new/equipment/motor-graders.html.

M Series 3 Motor Grader Specifications

  12M3/12M3 AWD 140M3/140M3 AWD 160M3/160M3 AWD  
Engine Model Cat C9.3 ACERT Cat C9.3 ACERT Cat C9.3 ACERT Less
Base Power (1st gear) - Net 133kW 179 hp 149 kW 200 hp 165 kW 221 hp Less
Base Power (1st gear) - Net (Metric)   181 hp   202 hp   224 hp Less
VHP Plus Range - Net 133-172 kW 179-231 hp 149-188 kW 200-252 hp 165-203 kW 221-272 hp Less
VHP Plus Range - Net (Metric)   181-234 hp   202-255 hp   224-276 hp Less
AWD Range - Net 141-188 kW 189-252 hp 156-203 kW 210-272 hp 172-219 kW 231-293 hp Less
AWD Range - Net (Metric)   192-255 hp   213-276 hp   234-298 hp Less
Moldboard - Blade Width 3.7 m 12 ft 3.7 m 12 ft 4.2 m 14 ft Less
Operating Weight, Typically Equipped 19 344 kg 42,647 lb 19 935 kg 43,950 lb 20 660 kg 45,547 lb Less
Operating Weight, Typically Equipped AWD 20 236 kg 44,614 lb 20 827 kg 45,917 lb 21 552 kg 47,514 lb Less

 

Image 1

Image 2

Note to Editors: Caterpillar rolls-out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

Press Inquiries

Cat Trade Press Media Representatives

Americas
Sharon Holling: Holling_Sharon_L@cat.com

Europe, Africa, Middle East
Francine Shore: Shore_Francine_M@cat.com

General Email: Cat_Trade_Press@cat.com

Reader Requests
www.cat.com/requestCatinfo