Three Ways to Boost Value of Preventive Mtce

Three Ways to Boost Value of Preventive Mtce

When you’re enjoying a busy work schedule with jobs lined up for months, you may be more focused on productivity than maintenance—but you also want to make sure your equipment keeps working with as few interruptions as possible. That’s where preventive maintenance (PM) practices come into play. Follow these three tips to keep your maintenance costs low and your uptime high.

1. Create, post and stick to PM schedules.

Construction accountants and financial advisors report that preventive maintenance schedules, when adhered to, are a best practice for maintaining the value of equipment and cutting down on repair costs.

2. Consider outsourcing as an efficiency booster.

Evaluate the maintenance and repair work your team is doing—what’s being done, the hours it takes and the cost of downtime. Also look at the time involved to schedule and manage product inventory. It’s possible you could save money and gain convenience by outsourcing certain maintenance tasks to a more efficient third party. If your shop is handling maintenance for equipment and vehicles, you may want to consider outsourcing one fleet.

3. Use technology to make maintenance as efficient as possible.

The machine hour meter records the number of hours the machine is “on,” but it doesn’t differentiate between “on time,” “working time” and “idle time.” Various monitoring systems do make that distinction, and this technology is integrated into many newer machines. When you can look at the data and see which hours are actually working hours, you can schedule maintenance using actual time worked. That means you can reduce the number of PMs needed annually.

Consider a machine with a recommended service interval of 250 hours and 70% working time. Approximately 30%, or 75 hours, of that 250-hour service interval is non-working time. That means every fourth PM is due to non-working hours alone, which isn’t a true indicator of usage. With more accurate data provided by technology, you can perform PMs when they’re needed and avoid unnecessary maintenance and associated costs.

Technology also helps you keep track of machine health—proactively—with alert codes that let the operator know when the machine is operating outside of normal parameters or needs service. The overall result will be fewer failures, less downtime and reduced costs.

Your Cat® dealer can offer a preventive maintenance program customized to your needs.

Research shows that creating, posting and sticking to preventive maintenance schedules is one of the best ways to reduce repair costs.

Customer Support Agreements

Every piece of Cat® equipment is designed and built to provide maximum productivity and operating economy throughout its working life. Your Cat dealer can help you maintain that built-in value through a Customer Support Agreement (CSA).

Learn More

Cat® Machines Cleanup Popular Australian Beach

Cat® excavators and multi terrain loaders work to reopen Bondi Beach, closed after a major storm, just days before a national holiday that brings tens of thousands of visitors to the popular Sydney, Australia destination.

Learn More