Caterpillar Expands EU Stage V, U.S. EPA Tier 4 Final Industrial Engine Range with New 9.3 Liter Offering

For Worldwide Release: December 2017 
Release Number: 657PR17

To address the diverse requirements of the global off-highway emissions landscape, Caterpillar has taken a customer’s approach to the new Cat® C9.3B industrial engine. Our customers expect reliability and durability, but they need it from a simpler, lighter package with more power and that’s what we’re giving them.

The 6 cylinder, 9.3 liter engine combines a new high-pressure, common rail fuel system and simplified air, electrical and aftertreatment systems to produce up to 340 kW of power and 2,088 Nm of torque out of a package that is nearly 140 kg lighter than its predecessor.

These changes will deliver many customer benefits including increased performance, improved fuel consumption and exceptional starting capability in cold climates.

These significant system upgrades, which provide added value to OEM customers, build on the core engine, which has been in production since 2011 with more than 46,000 engines, logging more than 150 million hours in real world off-highway applications. With a proven, reliable core engine and DPF (diesel particulate filter) solution already in place, Caterpillar’s focus for EU Stage V construction customers has been on simplifying design and improving performance.

Along with taking 39% of the aftertreatment packaging size out of the previous design, customers can opt for engine-mounted aftertreatment (EMAT) and full industrial power units (IPU) straight from the factory.

For the more challenging installations, remote-mounted aftertreatment is available that only requires wiring, coolant and diesel exhaust fluid effects added to the system.

With full engine production planned in the first quarter of 2018, Caterpillar is prepared to meet the needs of Stage V customers.

For more information on Stage V please visit or to learn more about our full range of engines and how they can help your business visit To find your local Cat dealer, visit

# # #

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2017 Caterpillar All Rights Reserved 

Press Inquiries

Caterpillar Trade Press Media Representatives


Sharon Holling:

Johanna Kelly:

Europe, Africa, Middle East

Francine Shore:

Reader Requests