New Cat® CG132B Natural Gas Generator Set Delivers Highest Efficiency in Output Category

New Cat® CG132B Natural Gas Generator Set Delivers Highest Efficiency in Output Category

For Worldwide Release: May 31, 2018

PEORIA, IL – Caterpillar Inc. today announced the release of the new Cat® CG132B, the first natural gas generator set in its class engineered to meet an electrical efficiency of 43.5 percent. Rated for continuous power at 400, 600 and 800 kW for both 50 and 60 Hz, this generator set is now available for public utility, agricultural biogas, landfill, sewage plant, and mining applications, along with industrial and/or commercial facilities.

With an updated package design, the CG132B introduces state-of-the-art components to increase overall plant efficiency. A flanged generator set concept includes a vibration-decoupled base frame to lower installation costs while improving reliability. The turbocharger is now water cooled and features a wider combustion air temperature window.

“The new CG132B was designed to increase efficiency and meet the evolving challenges of the power plant industry,” said Christian Oertel, product support manager. “The modified combustion chamber decreases knock sensitivity and pollutant emissions while also reducing service requirements.”

Oil change intervals have significantly improved due to enhanced oil management. Operation hours (oh) until the first major overhaul have been increased from 64.000 oh to 80.000 oh for natural gas applications allowing for more economical operation.

In addition, the CG132B features Caterpillar’s fully digitized Total Plant and Energy Management (TPEM) system. Responsible for controlling all power plant data within an advanced hardware and software solution, this new system eliminates the need for multiple controls. It also features a user-friendly 15-inch touchscreen, which provides a wide range of data concerning the status of the power plant. The data is saved for up to one year, enabling shorter maintenance times through systematic planning. The TPEM system meets the latest ISO 27001 standards.

“TPEM software provides comprehensive digital control over efficiency and performance. With complex applications and custom circuitry, modern energy plants require automation and closed-loop control with maximum operating security and seamless communication,” said Michael Dressler, product line manager.

Caterpillar is best in class in the power generation marketplace with market leading power systems engineered to deliver unmatched flexibility, expandability, reliability and cost-effectiveness. With parts and service available globally, Caterpillar offers worldwide product support through its comprehensive service and dealer network, where technicians are trained to service every aspect of the equipment.

For more information, visit https://www.cat.com/catcg132b or email electric_power@cat.com.

 

 

Available Images

Download here or contact Erin Collins at ecollins@gelia.com

Cat® CG132B Natural Gas Generator
Cat® CG132B Natural Gas Generator

# # #

 

Caterpillar Energy Solutions

With its two brands, MWM and Cat, Caterpillar Energy Solutions stands for highly-efficient and eco-friendly solutions for distributed power generation and manufactures gas engines, electricity power plants, as well as CHP plants. As part of the Caterpillar Global Power Solutions Division, Caterpillar Energy Solutions today commands a leading market position in the field of highly efficient, ecologically advanced distributed energy solutions. Thus, we serve our customers around the globe as a reliable partner for proven and sustained added value in the implementation of power plant projects. Our products are the result of more than 145 years of experience in the development and optimization of gas engines and generator sets for natural gas, biogas and other special gases.

About Caterpillar

For more than 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy, and natural resource assets. With 2017 sales and revenues of $45.462 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines, and diesel-electric locomotives. The company principally operates through its three product segments – Construction Industries, Resource Industries, and Energy & Transportation – and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

CAT, CATERPILLAR, BUILT FOR IT, their respective logos, “Caterpillar Yellow”, the “Power Edge” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2018 Caterpillar
All Rights Reserved

 

Press Inquiries

Sarah Pullen
Tel: +1 309 675 1513
Pullen_Sarah_C@cat.com

 

Reader Responses

Caterpillar Inc.
Electric Power Division
P.O. Box 0610
Mossville, IL 61552-0610