Cat® propel drive system upgrade for 7495 and 7495 HF shovels eases maintenance, reduces downtime and cuts costs

For Release Worldwide: August 2019 
Release Number: 493PR19

Caterpillar has developed a propel drive system upgrade for Cat® 7495 and 7495 HF Electric Rope Shovels. The upgrade reconfigures the crawler undercarriage to allow drive shaft and tumbler replacement from the outboard side, which improves access and decreases downtime by days. Improved component design extends durability and increases component life to reduce costs even further.

The new design slashes maintenance time and enhances safety by enabling access to drive components without removing the propel transmission. Additionally, Caterpillar engineered the upgrade to be a direct replacement. No machining of the crawler frame is required for installation.

The new design also is robust. Thrust loads are evenly distributed on large tapered roller bearings as opposed to bronze thrust plates, and the bearings are sealed and continuously purged with fresh grease to keep them free of contaminants. The result is increased durability in harsh environments and alignment with 25,000-hour planned rebuilds.

The propel drive system upgrade has operated successfully for thousands of hours in field validation. For more information, contact the local Cat dealer, or go to: www.cat.com/mining

 

# # #

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Trimble Navigation Limited, registered in the United States and in other countries.

©2019 Caterpillar. All Rights Reserved.

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

 Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Request
www.cat.com/requestCatinfo

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News
warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.