Caterpillar Produces 1000th 797 Ultra-Class Truck

For Worldwide Release: June 2018 
Release Number: 325PR18

Caterpillar recently celebrated the manufacture of the 1000th Cat® 797 Mining Truck. With 400 tons (363 tonnes) payload capacity, the 797F model is Caterpillar’s largest truck and the largest mechanical-drive mining truck in the world.

The 797 is the only mining truck in the size class to reach the 1,000 milestone. The first 797 placed in a mining operation was commissioned in 1999 and is still in service—with more than 130,000 hours working in Canadian oil sands. Extended durability has helped the 797 become a mainstay in Canadian oil sands operations. Since that time, the breadth of applications has grown to include copper, coal and iron ore mines—with the largest populations working in North America, South America and Australia.

“The 797 has proven its ability to deliver high production in the most challenging conditions—from the extreme cold and soft underfoot conditions of the Canadian oil sands to high altitude, deep pit copper applications in South America,” said Sudhanshu Singh, global product manager, large mining trucks. “In a broad range of applications, the 797F sets the production standard for ultra-class mining trucks. That’s a big reason why there are double the number of 797s at work today compared to the total number of all competitors’ trucks in the size class.”

The 20-cylinder, quad-turbocharged Cat C175 engine powers the 797F. Producing 4,000 hp (2983 kW), the C175 delivers more power for faster acceleration, faster speed on grade and greater productivity. For applications that don’t require the highest power, such as the flat hauls found in many coal and iron ore applications, a 3,550-hp (2647-kW) setting is available. A variety of fuel maps are available to balance productivity and fuel consumption, and a Tier 4 configuration is available to meet North American exhaust emissions standards. As with all Cat large mining trucks, the 797F features a complete power train designed and manufactured end-to-end by Caterpillar.

Caterpillar assembled the 1000th 797 and all of its predecessors at its Decatur, Illinois, USA, facility. The Decatur facility assembles all Cat large mining trucks.

For more information about Cat mining equipment and technology, contact the local Cat dealer or go to: www.cat.com/mining

# # #

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2018 Caterpillar All Rights Reserved

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas:

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East:

Francine Shore: Shore_Francine_M@cat.com

Reader Requests

www.cat.com/requestCatinfo

 

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.