Caterpillar
Caterpillar

Caterpillar surpasses 3 billion tonnes hauled autonomously by Cat Command for hauling trucks

 

 

For Worldwide Release: May 2021
Release Number:230PR21

Caterpillar announces an additional 1 billion tonnes of material hauled by autonomous trucks using Cat® MineStar™ Command for hauling, surpassing the 3 billion tonnes milestone. This achievement is joined by an expansion of the types of commodities hauled autonomously across a growing number of Cat mining truck class sizes, as well as other brands of mining equipment.

“Since surpassing the 2 billion tonnes milestone, we’ve equipped more mines with Command trucks and have established the world’s first gold mining application with Command for hauling,” offers Jim Hawkins, director of Cat MineStar Solutions. “Since surpassing 1 billion tonnes, we’ve expanded our Command fleet by nearly 250%.”

Caterpillar has Command autonomous haulage system (AHS) fleets operating across three continents – North America, South America and Australia – at 17 mine locations, operated by nine different customers. Commodities mined using the Cat Command include iron ore, oil sands, copper, coal and gold.

Command for hauling trucks now span class sizes from 190 to 360 tonnes (210 to 400 tons). The Cat line of Command models include the Cat® 789D, 793D, 793F, 797F and the 297-tonne (327-ton) 794 AC with electric drive. Command retrofit kits are available for Cat mining trucks as well as other brands of trucks and loading equipment. Since the first autonomous Cat trucks were commissioned in 2013, these AHS models have traveled more than 110 million km (68.3 million miles), equivalent to a minimum-distance, straight-line roundtrip journey to Mars, with no lost-time injuries associated with automated truck operation.

Customers using Command for hauling report significant gains in productivity and truck utilization rates with lower costs per tonne.  Customers have seen up to 30% higher productivity.

“We continue to decrease the time between our major milestone targets because, from initial contract to full deployment, we constantly improve Command implementation efficiency. Consistent with previous milestone trends, we anticipate crossing the 4 billion tonnes threshold at even a faster pace than achieving 3 billion tonnes,” says Marc Cameron, vice president, Caterpillar Resource Industries. “Looking forward, we are planning the expansion of Command for hauling to include our 140-tonne (150-ton) class Cat® 785 mining truck.”

More information on Cat Command for hauling trucks can be found by contacting a regional Cat dealer or visiting: https://www.cat.com

 

 

 

 

Cat 789D
of

Cat 789D

789D
of

789D

Cat 789D
789D

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

         

# # #

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2021 Caterpillar All Rights Reserved 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests

www.cat.com/requestCatinfo

 

 

 

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.