Caterpillar To Offer Dual Fuel Retrofit Kit for 785C Mining Truck

 

For Worldwide Release: November 2017 
Release Number: 587PR17

Caterpillar will offer its dynamic gas blending retrofit kit for the Cat® 785C Mining Truck. Cat Dynamic Gas Blending™ (DGB) technology allows engines to run on both diesel and liquefied natural gas (LNG). DGB lowers fuel cost while maintaining diesel power and transient performance.

“We’ve recently completed validation of the retrofit kit on the 785C Mining Truck with excellent results,” said Steve Igoe, commercial manager for Caterpillar’s Gas Engine Business. “The kit will allow customers to reduce fuel costs significantly by using LNG. Natural gas and LNG offer both economic and environmental benefits to the mining industry.”

The 785C Retrofit Kit is the first DGB system Caterpillar has offered for mining machines, and it will be available for purchase in January 2018 from the global Cat dealer network. Caterpillar will offer additional DGB systems in the future.

“The retrofit kit is built on proven Cat DGB technology and has been used in the oil and gas industry since 2013. The retrofit kit offers a peak substitution of up to 85 percent of diesel with natural gas and gets the same performance, reliability and payload as a diesel truck,” said Igoe. “This will allow our customers to realize a 20 to 40 percent savings on fuel costs, which can represent millions of dollars each year for a large mine.”

To learn more about dynamic gas blending, stop by the Caterpillar exhibit, #424, at the High Horsepower Summit, November 6 – 9 in Jacksonville, Fla. Caterpillar experts, including Steve Igoe, will be there to explain this innovative, cost reducing technology.

# # #

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2017 Caterpillar All Rights Reserved

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests www.cat.com/requestCatinfo

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.