Cat® R1700 XE LHD
Cat® R1700 XE LHD

Caterpillar to unveil new Cat® R1700 XE LHD battery electric vehicle with MEC500 Mobile Equipment Charger at MINExpo

 

For Worldwide Release: June 2021
Release Number: 482PR21


Underground mining continues to be an early adopter of sustainable mobile equipment solutions, based on the need for a clean and safe working environment. The new Cat® R1700 XE LHD, with its 15-tonne payload and 24,190-kg lift and tilt breakout, features a battery electric design that delivers superior productivity in underground applications with the benefits of no engine heat or exhaust emissions. It offers an 18 km/h top speed.

The new Cat LHD offers 100% battery electric propulsion, which generates significantly less heat. An Autodig function optimizes loading and traction control to extend tire life. Liquid cooling allows the batteries to be cooled while the machine is put back in operation, increasing machine uptime availability.

To maximize runtime, batteries stay on the machine. Using the portable Cat MEC500 Mobile Equipment Charger, the R1700 XE can be fully charged in less than 30 minutes using a single charger or in less than 20 minutes using two chargers.

There is a need for a clean and safe working environment underground, which currently requires installation and maintenance of complex and expensive ventilation systems for clearing exhaust emissions. With less emissions from the machines like the new Cat R1700 XE, mines can reduce the dependency on these ventilation systems. The new R1700 XE LHD is a key part of the vision to an all-electric mine. It is the first battery powered/zero emissions equipment for the underground hard rock mining LHD (Load Haul Dump) product line and offers remote control operation capability.

MEC500 Mobile Equipment Charger

A first of its kind in the industry, the new Cat MEC500 Mobile Equipment Charger is designed to charge quickly and safely wherever it is needed. Unlike static charging stations, the 1600-kg portable charger can be moved to where it is needed via towing, fork truck, or the R1700 XE. It eliminates the need for regular battery handling and swapping, allowing for more efficient charging and production.

Its 500kW capability delivers an impressive range of 300-1,000 Volts and up to 700 Amps. This fast charger can be used as a single unit to deliver a full charge to the R1700 XE in less than 30 minutes or in parallel to charge the LHD in less than 20 minutes. Its adjustable output voltage and current can trickle charge the battery, maintaining optimal performance for the R1700 XE.  

The charger is built rugged meeting ISO2867 rockfall protection and IP66 rating for water and dust protection. Key components are isolation mounted against vibration or seismic activity. It is sealed against humidity with enclosed air conditioning.

MINExpo 2021 attendees will get a first look at the R1700 XE and MEC500 this September in the Caterpillar Central Hall exhibit 6229 at the Las Vegas Convention Center.

 

 

Cat MEC500 Mobile Equipment Charger
of

Cat MEC500 Mobile Equipment Charger

Cat MEC500 Mobile Equipment Charger
of

Cat MEC500 Mobile Equipment Charger

Cat R1700 XE
of

Cat R1700 XE

Cat R1700 XE
of

Cat R1700 XE

Cat MEC500 Mobile Equipment Charger
Cat MEC500 Mobile Equipment Charger
Cat R1700 XE
Cat R1700 XE

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

         

# # #

 

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2021 Caterpillar All Rights Reserved 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests

www.cat.com/requestCatinfo

 

 

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.