Design Refinements for New Cat® Articulated Trucks Address Operator Safety and Convenience, Enhanced Control, and Powertrain Advances

For Worldwide Release: April 2018 
Release Number: 259PR18

Three new Cat® articulated trucks—730, 730 EJ (Ejector), and 735—have been extensively redesigned, enhancing the field-proven features and performance of their C-Series predecessors (730C2, 730C2 EJ, and 735C) with new operator stations—including innovative new controls, transmission-protection features, new hoist-assist system, advanced traction control system, new stability-assist system, and a fuel saving ECO operating mode.

In addition, the design of the 730 and 730 EJ is enhanced with automatic retarder control and a hill-start feature. The 735 retains these features from its C-Series predecessor and further incorporates significant design refinements that include a new Cat® C13 ACERT™ engine, Cat CX31 transmission (also on the 730 and 730 EJ) and structural and dimensional modifications that reduce empty weight by 22 percent, while retaining the productivity of the outgoing 735C. These features combine for an up to 19-percent gain in fuel efficiency.

Operator station

The cab's new external “spinal-ROPS" design incorporates a rear-quarter glass that eliminates a structural pillar in the C-Series design, for enhanced rear visibility. Also, a new “wake-up” feature initiates the machine's displays when the door is opened. The door is of a lighter, stronger design with a shut-assist feature for improved sealing against dust infiltration. The overall cab design results in lower inside sound levels at 72 dB(A), a 7 dB(A) reduction compared to previous models.

Optional new infrared glass reduces solar heating inside the cab, and left- and right-hand sliding windows increase ventilation and facilitate communication with workers and the loading-vehicle operator. A new, automatic climate-control (HVAC) system positions more vents above and behind the operator for increased heating and cooling efficiency. A new heated/cooled seat is designed to give operators increased adjustments that allow "dialing in" personal-comfort settings; also, the passenger seat now uses a flip up/down design and added cushioning.

 For added safety, a new lighting system, controlled via a ground-level switch, illuminates the cab's entry steps and hitch area. Optional integrated payload lights provide an external indication of payload levels for the loader operator. Optional long range, LED work lights improve visibility at night or in situations of lower visibility. New cab-mounted mirrors, including a front-visibility mirror, enhance all-around visibility for the operator. Exterior cab features include an improved flexible lower fender and a low-profile exhaust stack that need not be removed for transport.

The optional Cat Connect PAYLOAD technology calculates payload via sensors on the walking-beam suspension, and load-status lights at all four corners of the cab roof ensure visibility to the loader operator from any angle. In addition, the standard Cat Detect/Stability-Assist system monitors the working angle of the tractor and body, as well as the grade, and cautions the operator if the machine is approaching the set threshold angle, stopping the dump process if continued action may result in potential tipping.

Further enhancing safe operation is the Cat Advanced Automatic Traction Control system, which features refined technology for proactively applying differential locks to avoid wheel spin. Also, a "terrain-based," throttle-smoothing system prevents acceleration surges when traveling over extremely rough terrain that makes keeping a steady pressure on the throttle pedal difficult.

Innovative controls

A new combined transmission-and-hoist lever provides efficient, single-lever control of vehicle speed and body-hoisting functions to reduce operator effort and to automate repetitive operations. A switch in the cab allows operators to choose either manual or assisted hoisting control, the latter selection automatically applying the waiting brake, shifting the transmission to neutral, and raising the body to maximum angle at engine high idle. Assisted hoisting returns the body to the lower position at the flick of a switch. Both raise and lower functions feature automatic cushioning and speed reduction at limits of movements.

New buttons in the combined transmission and hoist lever allows setting (limiting) machine speed and selecting the transmission waiting brake. In addition, a new shift-protection system brings the truck to a safe stop if a directional shift is made while the truck is moving. The new combined shifting/hoisting lever also incorporates a parking position. A tertiary brake switch sets the parking brake in the unlikely event of main and secondary braking malfunction

Model specifics

The new 735 replaces the Cat C15 ACERT engine, rated at 441 net horsepower, with the Cat C13 ACERT, rated at 428 net horsepower. The new 730 and 730 EJ continue to use the Cat C13 ACERT engine, rated at 367 net horsepower. The C13 engine used in all the new trucks is available in configurations to meet emissions standards of both highly-regulated and lesser-regulated countries.

The 730 EJ is designed to eject loads while traveling, providing positive dumping of the entire load, and also to work in areas with overhead restrictions and with soft underfoot conditions with improved machine stability.

 

Cat 735 articulated truck.

Specifications

 

730

730EJ

735

Engine

Cat C13 ACERT

Cat C13 ACERT

Cat C13 ACERT

Max Net Power @ 1,700 rpm (SAE J1349)

367 HP (274 kW)

367 HP (274 kW)

428 HP (319 kW)

Weight (empty)

26.3 tons (23,900 kg)

29.3 tons (26,600 kg)

27.8 tons (25,240 kg)

Rated Payload Capacity

30.8 tons (28,000 kg)

31.0 tons (28,120 kg)

35.2 tons (32,000 kg)

 

Wheel Base

8 ft 9” (2679 mm)

8 ft 9” (2679 mm)

8 ft 9” (2679 mm)

Number of Axles

3

3

3

Drive Configuration

6-wheel

6-wheel

6-wheel

# # #

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Trimble Navigation Limited, registered in the United States and in other countries.

©2018 Caterpillar All Rights Reserved

 

Print Media

Placeholder image


Download High Resolution Image

Cat 735 articulated truck.

 

Placeholder image


Download High Resolution Image

Cat 730 and 735 articulated trucks

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests www.cat.com/requestCatinfo

 

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.