New Cat® Durilock™ Shroud System
New Cat® Durilock™ Shroud System

New Cat® Durilock™ Shroud System for underground loader buckets cuts maintenance time and allows fast adaptation to application needs

 

For Release Worldwide: September 2020
Release Number: 733PR20

Caterpillar has developed the new Durilock Lip Shroud System for underground loader buckets. The fully integrated bucket system features hammerless installation and maintenance-free retention of ground engaging tools (GET) with Cat® Infinitite elastomer compression retainers. Three interchangeable shroud styles enable a mining operation to quickly remove one type and replace with the type that is best suited to the loader application—without changing the base edge or retention system.    

The Durilock system delivers 50% faster installation and removal of GET compared to legacy, mechanically attached systems, and, because there is no need to re-torque bolts periodically, maintenance time for GET is reduced by more than 50%. Additionally, integral corner guards extend bucket in-service time by about 30%.

The Durilock Shroud System is available for Cat R1700 to R3000 loaders and most buckets of 5 to 10 cubic meters capacity.

Innovative, adaptable GET

The Cat Infinitite retention design provides superior retention reliability without time spent performing re-torque procedures. The elastomer compression retainer installs in seconds to allow fast installation and removal. There is no complex hardware to fail, handle or tighten.

The Durilock system offers three different shroud styles to enable matching the GET to the application and conditions in the mine. The D50S Standard is a traditional wedge shape used in most production and development applications. The D50A Abrasion has a contoured design and repositions more material on the shroud base, and the D50P Penetration has less leading-edge material to deliver easier penetration in dense material.

The lip assembly provides the mounting surfaces for the shrouds and corner protectors, which balance corner and center station wear rates. Cast corners are welded to the base edge assembly to create the lip assembly. The corners incorporate a stepped design that eliminates corner shroud torsional loads and delivers superior reliability. The integral corner design boosts corner life by 15% and improves penetration as compared to systems that experience corner erosion and shortened bucket life due to corner rounding.

With the addition of Durilock, Caterpillar has a complete portfolio of GET products that are designed to meet the unique and challenging requirements of any underground mine. For more information about Durilock and Cat GET offerings for underground loaders, contact the local Cat dealer.

 

 

 

963
of

Cat Durilock GET on underground loader bucket

963

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News

 

# # #

 

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2020 Caterpillar All Rights Reserved 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests
www.cat.com/requestCatinfo

 

 

warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.