7495

Updated AC electric drive system boosts reliability and safety of Cat® 7495 and 7495 HF Electric Rope Shovels

For Release Worldwide: November 2019 
Release Number: 902PR19

Caterpillar has updated the proven AC electric drive system for Cat® 7495 and 7495 HF Electric Rope Shovels to deliver even greater reliability, improved maintenance access, enhanced safety and expanded ability to perform at high altitudes and in extreme temperatures. The updated system also is designed to easily integrate with advanced technologies.

“Caterpillar and our predecessor in shovel design and manufacturing, Bucyrus, have supplied more than 300 AC electric rope shovels,” said Dale Blyth, product manager, electric rope shovels. “The most recent advances in AC drives are integrated in this update and demonstrate how we apply our experience to help customers lower cost per ton and bolster safety.”    

Updates include a liquid-cooled motion regulator cabinet for more efficient dissipation of heat generated by electrical components. The new system enables shovels to operate at temperatures of -40 degrees C/F to +50 degrees C (122 degrees F) and altitudes of 5 250 meters (17,220 ft) without derating. The reliable system also eliminates airborne contaminants in the cabinet and lengthens service intervals—for reduced costs and greater uptime. Additionally, a new, faster propel transfer switch cuts lag time by 75 percent for improved productivity.

New technologies enable consolidating two cabinets in the machinery house to create space for easier maintenance access. The updated maintenance station is designed for integration of current and future technology solutions, including Cat MineStar.

The drive system design uses common motors in multiple applications. That means fewer parts to stock, improved parts availability and simplified maintenance. The new motors have higher power densities, smaller frame sizes and optimized footprint, which aids access.

The Cat rope shovel electric drive system still features proven elements such as fuseless insulated-gate bipolar transistor (IGBT) modules. And the on-board maintenance station still aids technicians in identifying faults and resolving issues.

The new electric drive system will be on all new production 7495 and 7495 HF shovels beginning in late 2020. The system is not intended for retrofit, though some elements, such as the fast propel transfer switch, are available as upgrades to machines already in service.

For more information, contact the regional Cat dealer or go to: www.cat.com/mining.

 

# # #

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2019 Caterpillar All Rights Reserved 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

   Sharon Holling: Holling_Sharon_L@cat.com

   Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

    Francine Shore: Shore_Francine_M@cat.com

Reader Requests
www.cat.com/requestCatinfo

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News
warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.