Cat® Tiltrotator gives Swedish contractor competitive edge

Cat® Tiltrotator gives Swedish contractor competitive edge

Börje Holmgrens Åkeri in Björklinge outside Uppsala is one of the first contractors in Sweden with Caterpillar's new tiltrotator system, TRS.

 

”We chose the Cat® tiltrotator because it feels convenient that all comes from one and the same manufacturer. Because everything is prepared from the factory, I think the equipment will harmonize better with the machine as well”, says Stefan Holmgren

The new tiltrotator, TRS 10 is mounted on the company's brand new wheeled excavator, the Cat M316F.

"My expectations are that it should work without any worries and if something is needed it is just one supplier I can turn to.

TECHNOLOGY IMPORTANT

Stefan says that a part of the company's strategy is to use new technology.

"We become more efficient and get competitive advantages. One example is our hybrid excavator Cat 336E that made us save 20% fuel compared to the previous machine and that also means a lot.

ABOVE THE EXPECTATIONS

Stefans father Börje started the company at the end of the 1980s, it was converted into a limited liability company ten years later and then Stefan bought it in 2008. The company currently has 32 employees and a turnover of SEK 80 million.

A success factor is to provide high service.

"We do what we promise and our ambition is to deliver a better result than the customer expects. We have short decision-making ways and are an independent company that is not affiliated or part of a larger organization. We are perceived as fast.

Börje Holmgrens Åkeri is both a construction company and a haulage contractor. The main customers are Skanska, Veidekke and Sh building. Right now most of the resources are involved in the big project Östra Fyrislund. At the E4 in southeastern Uppsala a 70,000 square meters large area is being built for commerce, office and industry.

 

CAT FOR WHOLE COMPANY

All construction machinery in the company is from Caterpillar.

"The machines are robust, reliable and there is rarely something wrong with them. We are very pleased with the service from dealer Pon and we always work well together”.

At Pon we do our utmost to make the operator’s life as comfortable as possible so that they can do their job quickly and efficiently.”says Anders Forsberg, product manager Pon Sweden

Machinery:

Crawler excavators: Cat 336E hybrid, Cat 329E

Wheel excavators: Cat 315D, Cat 316F

Dozer: Cat D6 T and Cat D6 N. Both LGP, Cat D4 H

Dumper: Cat 730

Wheel loader: Cat 924K and Cat 924H

Trucks: 23 pcs

CAT TILTROTATOR TRS-SERIES

The Cat tiltrotator models offer 360° degrees rotation and 2 x 40° tilting which dramatically reduces machine movements (i.e. fuel consumption) while being able to reach most places from one single position. The Cat tiltrotator enables to manoeuvre around posts, rocks, or other obstacles and along ditch edges. And can work over, under, and around all types of obstructions or infra-structure using any attachments or tools required for the job.

 

GET THE LATEST STORIES AND TIPS FROM CATERPILLAR – SIGN UP FOR OUR E-NEWSLETTER

 

 

RELATED STORIES:

 


6 Tips for Boosting Productivity with Attachments


How do you choose the work tools that create the optimal pairing with your machine? These six suggestions will help you achieve the best productivity for your money.

Get Tips

6 Tips for Boosting Productivity with Attachments


How do you choose the work tools that create the optimal pairing with your machine? These six suggestions will help you achieve the best productivity for your money.

Get Tips
U.S. Recycler Boosts Daily Productivity Using Cat® Scrap Shear

Better productivity, service and resale value—that’s why Rivers Edge Scrap Management relies on Cat® machines and work tools. The recycler’s experience with the new S3070 scrap shear is no exception.

Learn More
Company Gets Extra Day of Work Out of Cat Hammer

Productivity gains of up to 20%, fuel savings and happier operators—all from a work tool? According to KJ Services Ltd of South Wales, that’s what the new Cat H130Es hammer delivers.

Learn More
Transporting a 100-Tonne Machine 750 Meters Below the Surface

Thrilled with the performance of its Cat 992G wheel loader, K + S Rohsalz decided to purchase a 992K. But getting the new machine down the German salt mine’s Surface of narrow material shaft was no easy task.

Learn More
Cat® H180ES Hammer Breaks New Ground In Norway

The Cat® H180ES Hammer is helping to clear the way for Norway’s largest ongoing infrastructure project.

Learn More