Van Heck Water Displacement

Powered by the Cat® C27 and C32

Van Heck moving water
Van Heck moving water

Van Heck HK700 and HK800 Mobile Pump Unit 

Moving Water Any Way You Want It

For more than 60 years, the Van Heck Group has grown from a one-man dredging operation into a family-owned global leader in water control solutions. With a versatile, high-capacity rental fleet, Van Heck supports industries worldwide, from offshore wind farms to large civil works. They specialize in high-volume, high-pressure water displacement, and their mobile pump units are powered by the reliable Cat® C27 and C32 engines.

Van Heck Logo
Van Heck Logo

POWER PROFILE

CUSTOMER:

Van Heck

LOCATION:

Netherlands

EQUIPMENT

HK 700 and HK800 Mobile Pump Units

PRODUCT:

C27 & C32

DEALER

Zepplin Power Systems

SECTOR

Industrial Power

        

UNDER PRESSURE

Customers choose Van Heck for their rapid response time, wide range of capacities, 24/7 global assistance and innovative, customised solutions. Because they have such diversity in pump units, Van Heck can handle everything from dredging, salvage and offshore operations to sewer renovation, cooling water applications and floodings.

Similarly, when Van Heck rents out a machine, they know it will be running nonstop. In 2015, Van Heck deployed 20 HK700s to Serbia to drain a flooded coal mine. The mine was Serbia’s main energy source for power production, so efficiency was essential. Powered by Cat® C27 engines, the machines ran 24/7 for nine consecutive months, draining 150 million m³, or 5.3 billion cubic feet of water. That amount is equal to 60,000 Olympic swimming pools, or more than 25% the volume of the Suez Canal.

Recently, Van Heck sent three of their largest units, the HK800s (9000m³ per hour / 5300 cfm at 4.3 bar / 62 psi) along with three HK700s, (7000m³ per hour / 4120 cfm at 3.2 bar / 46 psi) to build a new port in Saudi Arabia. The HK800s were powered by the Cat C32 EU Stage V, while the HK700s used the Cat C27. The machines ran for an uninterrupted 18 months at extreme temperatures of 50 °C/122 °F, again proving their durability. “Redundancy or breakdowns are not an option,” says van Dijk. “So, choosing Cat engines is a very deliberate choice.”

FURTHER INVESTMENT IN EXPANDING THE FLEET

Van Dijk recently invested in 17 new Van Heck machines with Cat C27 Stage V and C32 Stage V engines, confident their power, reliability and emission compliance can drive high-flow, high-pressure water solutions. Due to ever-increasing demands and sparse deck space, Van Heck squeezes an enormous amount of power into a 20-ft container frame, supplying high-volume, high-pressure power in the smallest possible footprint.

Caterpillar worked with Van Heck to design the correct cooling systems for the pump unit, ensuring it could run 24/7 in extreme heat. “We’re obviously heavily investing in the cleanest, most efficient technology available,” says van Dijk. “Since we only rent – we never sell – we need the most reliable, fuelefficient, clean-as-possible pump units to supply either high-volume or high-pressure water to our customers. That’s why we choose Cat engines.”

Over the years, Van Heck and Zeppelin Power have built a strong and successful partnership together. With factory acceptance testing in house, Van Heck leans on the dealer to select the ideal engine for their operations and ensure deliveries are on time. “Our customers are definitely happy with the pump units we supply because all our diesel-driven pumps are powered by Cat engines,” says van Dijk. “We operate worldwide, from Australia to North America, from Saudi Arabia all the way up to Norway, and we need that global presence and support. So, it’s a very deliberate choice we’ve made.”
 

“Reliability is the main reason customers choose Van Heck, and it’s why we choose Caterpillar.”

Herman van Dijk, Owner, Van Heck  

of

Van Heck, a leader in water control, uses Cat® engines to power its mobile pump units for demanding projects worldwide. Their reliable, high-capacity pumps help tackle everything from flood recovery to port construction, proving the value of strong partnerships and innovative engineering

Van Heck case study

Read how Caterpillar and Van Heck are teaming up to keep high-pressure water operations flowing. 

Download Now
Van Heck Profile Document
Van Heck Profile Document

Cat Industrial Engine Support

Your Cat dealer is your go-to resource for everything from installation support to troubleshooting to in-the-field service. With 171 dealers serving 192 countries, the expert assistance you need is always close at hand. 

Customer Value Agreement (CVA)

Our Cat Customer Value Agreement provides a comprehensive package for your engine’s entire lifecycle, covering parts, services and cutting-edge technologies. We manage costs no matter the stage of your fleet’s lifecycle with a hassle-free service plan so you can focus on what really matters. 

Find Your CVA
Engine repair person in safety vest holding tool.
Engine repair person in safety vest holding tool.

Digital Services

Optimizing the lifecycle of your Cat engine is made easy with our integrated suite of digital services. Gain complete visibility and actionable intelligence on your engine fleet’s health to ensure your jobsite is operating at its best.

Learn more
Customer using phone to use Digital Services
Customer using phone to use Digital Services

Why Use Genuine Cat® Parts?

Through the global Cat Dealer Network, you gain access to the full suite of proactive fleet maintenance services, backed by Genuine Cat® Parts to maximize efficiency and sustainability over the lifetime of your equipment.

Parts and Repair Options
Man in safety helmet and protective gloves cleaning engine components.
Man in safety helmet and protective gloves cleaning engine components.

Contact your local dealer

Want to learn more about Cat industrial engines or related products or services?

Contact dealer

TIPS AND INFORMATION

INDUSTRIAL POWER E-NEWSLETTER

Sign up for our e-newsletter for more customer profiles, along with the latest industry news and expert tips.

Sign-up