Texas Pump Systems
Customizable Pump Packages

Powered by a Cat® C32 Industrial Engine

POWER PROFILE: Texas Pump Systems Customizable Pump Packages

Pumping Up The Innovation

Customized Pump Packages

Texas Pump Systems (TPS) was founded in 2014 in Stephenville, Texas. When it comes to crafting pump packages, they’re far from an assembly line. The company specializes in customizing one-off products that meet the ultra-specific needs of clients—for everything from steel mills to drilling operations to water disposal (and a whole lot in between).

Texas Pump Systems logo

Product Overview

Cat Engine Overview

Read profile

Gallery

Related Profiles

PRODUCT OVERVIEW

  • When Texas Pump Systems needed to build pump packages for use in explosive atmospheres, they relied on Caterpillar’s hazardous-area certified engine by pairing it with their own custom-control systems, monitoring, gauges and so on. 
  • Twenty years ago, Caterpillar saw the need for engine compliance with an explosive- atmosphere design, inspiring changes like adding exhaust gas coolers to keep surface temperatures down to 200 degrees and creating a safe work environment which is key to keeping employees at work and productive.
  • TPS was able to dramatically increase pump horsepower from 700 to 1300 by using the Cat® C32 industrial power unit. 
  • The global Cat dealer network provides added value for customers by supplying accessible, unparalleled parts and service including 24/7 online parts ordering access.

Check the specs

Contact Texas Pump Systems

CONTACT YOUR CAT DEALER

Product image
of
Product image

Cat® Engine Overview

  • The Cat C32 industrial engine is offered in power ranges up to 1200 hp (895 kW) and peak torque 5500 Nm (4056 lb-ft) and allows for platform downsizing while maintaining reliability and durability.
  • The C32 engine is ideal for tough industrial and construction applications such as dredges, chippers, grinders, emergency water pumps and rock drills among other applications requiring continuous peak performance under the most demanding conditions.
  • The key to success for any machine is avoiding downtime as much as possible. Thanks to the DEF-free, dual-can DOC with transparent regeneration offered by the 32 engine, operators can stay focused on being productive for the long haul.
  • When it comes to making the engine installation process smoother for Original Equipent Manufacturere (OEMs), look to the C32 engine. Using innovative technology solutions, the C32 was created to eliminate the need for thermal management and Diesel Exhaust Fluid (DEF), reducing the size of the overall engine package. And thanks to flexible aftertreatment mounting options, installing such a large engine just got a lot less complicated.
  • Optimized to meet some of the most demanding operating cycles of just about any machine, the DEF-free Cat C32 helps owners and operators save on operating costs while also remaining maintenance-free for the engine's lifetime.

 

C32 Industrial Engine
of
C32 Industrial Engine

Compare Models

POWER PROFILE

CUSTOMER:

Texas Pump Systems

PRODUCT:

Customizable Pump Packages

LOCATION:

Stephenville, TX

SCOPE OF ENGINE USE:

Cat® C32 Industrial Disel Engine

DEALER:

Holt Cat

Avoiding Fireworks

Safety first. We all learn that on day one, regardless of where we work. But imagine if you worked on an offshore oil rig. When you’re miles out at sea, safety is absolutely everything. Texas Pump Systems creates customized pump packages for clients around the world—including oil companies that need pumps for floating production and storage facilities. This equipment is used for “pigging,” which entails pumping fluid from the seabed into vessels that hold a couple million barrels of crude oil. Obviously, it makes for quite an explosive atmosphere.

“Using diesel engines in that particular application causes for a lot of headache, because you can imagine with these engines sitting on two million barrels of crude oil—one spark will make a pretty good firecracker,” explains Ernst Vanderlaan, General Manager of Texas Pump Systems. Not surprisingly, achieving a perfect combination of safety and performance was a pretty sizable hurdle to overcome. Twenty years ago, requirements for engine compliance when it came to usage around hazardous explosive materials was lax at best. But Caterpillar saw the need for explosive-atmosphere design and got to work. Innovative engine design inspired changes like adding exhaust gas coolers to keep surface temperatures down to 200 degrees. 

So when Texas Pump Systems got the call to build pump packages for use in explosive atmospheres, they were able to rely on Caterpillar’s hazardous-area certified engine to be used at the heart of their assembly. By pairing that with their own custom-control systems, monitoring, gauges and so on, Texas Pump Systems was able to deliver top-of-the-line packages that would not only get the crucial job done, but also keep all those hard-working folks (and their well-earned sea legs) completely safe. 

The Need For Speed

Texas Pump Systems was founded in 2014 in Stephenville, Texas. When it comes to crafting pump packages, they’re far from an assembly line. The company specializes in customizing one-off products that meet the ultra-specific needs of clients—for everything from steel mills to drilling operations to water disposal (and a whole lot in between). “I really don’t think there’s anybody else that does engine-driven packages like we do,” Vanderlaan says. “Every application requires a different configuration, so every pump system requires a different configuration. If you package the stuff right, it’s going to last a long, long time.”

That affinity for creative thinking came in quite handy when Texas Pump Systems’ existing customer Graco Oilfield Services came with a new request. Graco has been a pioneer in the higher horsepower market, being the first ones to use 700 hp pump packages in their well servicing. Come 2019, they were looking to dramatically up their game to 1,300 hp application, which nobody had done before. The envelope-pushers at Texas Pump Systems made it happen with a Cat® C32 industrial power unit (IPU) at the heart of the package. The designers chose the C32 specifically because of its reduced size and weight—not to mention its extreme reliability and affordability. 

The big challenge was to fit an automatic transmission behind the engine and keep the cost down for the customer. Vanderlaan’s team solved the issue by using new C32 engines paired with rebuilt transmissions and high-pressure pumps to minimize the expense. So not only did Graco save money, but their new packages allow them to complete jobs much faster than the lower horsepower machines—and also achieve a deeper horizontal lateral while they’re at it (up to 5,000 feet with the latest pumps). Talk about a win/win for everyone.

“I work a little different. I think one-offs are challenging—they’re fun,” says Vanderlaan. And with these pump-packaging puzzles to constantly solve, the Texas Pump Systems team works closely with their Caterpillar dealer, Holt Texas, to brainstorm completely outside-the-proverbial-box unique solutions and answer the (literally) powerful questions. That way clients know that their customized packages are one-of-a-kind and more than ready to work. “When Holt says Caterpillar is a family, they truly mean it,” Vanderlaan explains. “It takes a village, and they’ve always been such a resource—even friends—for us.”  

“I DON’T EVEN SEE CATERPILLAR AS A VENDOR ANYMORE - THEY’RE PRETTY MUCH PART OF OUR COMPANY. WE’RE FAMILY.”

 

DOWNLOAD PDF VERSION
OF POWER PROFILE

Want to share this story? Download a PDF of this Cat Industrial Engine Power Profile.

Download Power Profile
Download PDF

POWER PROFILE IMAGE GALLERY

Image 1
of
Image 2
of
Image 3
of
Image 1
Image 2
Image 3

Cat® Industrial Engine Support

Your Cat® dealer is your go-to resource for everything from installation support to troubleshooting to in-the-field service. With 171 dealers serving 192 countries, the expert assistance you need is always close at hand.

Customer Value Agreements (CVAs)

We may be an engine supplier, but supplying an engine is just part of our commitment to you. We also offer support. Long before a product ever rolls off your assembly line, our application teams — both at the factory and at your local Cat dealer.

Learn more
Customer Value Agreements (CVAs)

Digital Services

Through Cat digital services, you gain access to robust software and hardware solutions designed to maximize fleet efficiency - backed by Caterpillar’s unmatched network of experts. Gain the insight you need to make decisions on the fly to secure the health of your equipment and minimize nonproductive time.

Learn more
Digital Services

Why Use Genuine Cat Parts?

Looking for 24/7 access to information on the Cat parts, tools and materials you need to get the job done? You'll find it on the new parts.cat.com. 

Learn more
Why Use Genuine Cat Parts?

Contact your local dealer

Want to learn more about Cat industrial engines or related products or services?

Contact dealer

INDUSTRIAL POWER E-NEWSLETTER

Sign up for our e-newsletter for more customer profiles, along with the latest industry news and expert tips.

Sign-up