For Worldwide Release: January 8, 2018
Release Number: EEPR0118
Award-winning Clean Energy Plant at Monogram Foods Features Cat CG132-08
PEORIA, IL – Caterpillar Inc. supplied a Cat® CG132-08 gas generator set to power a clean energy plant at Monogram Foods, which was recently recognized as the “Biogas Project of the Year” by the American Biogas Council.
The Biogas Project of the Year honors an operation that strongly exemplifies financial ingenuity, energy efficiency and sustainable waste treatment.
The Cat CG132-08 gas generator set was built in Mannheim, Germany and delivered to Monogram Foods as a complete package with the generator set and switchgear installed in the enclosure.
Within this clean energy plant, waste is broken down in the digester and converted to methane gas, which is used to fuel the generator set that is capable of producing 400 kW of electric power. The bioenergy production capacity reduces net carbon emissions by 2,687 metric tons per year by reducing the use of fossil fuel-derived electric and natural gas for heating.
“We knew we had to treat the wastewater and it would produce methane. Either we had to just burn it in a flare – but you can’t release methane into the atmosphere – or get a Cat generator set and run it on methane. So now we’re producing heat and electricity, and it’s a win-win for everyone,” says Brian Neal, manager of environmental health and safety for Monogram Foods.
Carolina Cat Power Systems provides technical support and period maintenance to the project, including checking spark plugs for wear, conducting voltage regulator checks, greasing the generator bearings and taking coolant and oil samples.
For more information, visit www.cat.com/powergeneration or e-mail cat_power@cat.com.
Download here or contact Kellie Mazur at kmazur@gelia.com
# # #
About Caterpillar
For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Power Systems - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
CAT, CATERPILLAR, BUILT FOR IT, their respective logos, “Caterpillar Yellow”, the “Power Edge” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2018 Caterpillar
All Rights Reserved
Press Inquiries |
Kellie Mazur Aljoscha Kertesz |
Reader Responses | Caterpillar Inc. |