Cat® GSH420/GSH520 Grapples Feature Design Refinements for Effectively Handling Bulk Materials

Cat® GSH420/GSH520 Grapples Feature Design Refinements for Effectively Handling Bulk Materials

For Release in North America, Latin America, Europe, Africa, Middle East: June 2018 
Release Number: 334PR18

The new Cat® GSH420 and GSH520 orange-peel grapples, replacing the GSH15B Series grapples, are designed for a wide range of applications, including handling shredded scrap, such as long structural beams and car bodies; handling rocks at construction sites; and waste at recycling and transfer stations. The performance and efficiency of the new Cat grapples help waste-handling operations, in particular, meet the challenges of increased environmental regulation, growing pressure to recycle a mix of materials, and stringent budgets.

The new grapples feature horizontal placement of the cylinders, thus creating a profile that allows for effective material penetration and efficient bulk-material handling. The design enhances the strength, reliability, and durability of the new grapples, which are available in four-tine and five-tine shell configurations and in closed or semi-open versions. In addition, the GSH420 and GSH520 feature a redesigned rotation system. The new grapples are designed to work with the Cat MH3022, MH3024, and MH3026 material handlers.

Long-term durability

The design of the GSH Series grapples features construction of high-grade, impact-resistant steel that protects vulnerable areas, such as hydraulic cylinders. For added durability, high- quality bushings with lubrication grooves and hardened pins are used in all pivot points. Tines are configured with replaceable cast tips made from BHN 445-555 material that resists wear.

In addition, solid hinge-point construction and robust end-stops ensure long service life, and routing hydraulic hoses within the tines reduces hose wear. All mounting brackets feature a solid pin to keep the bracket in an upright position for ease of installation. Also, the new GSH grapples feature a standard lifting eye on the bottom of the housing for expanded versatility, such as mounting a magnet.

The new HR10 rotation group, featuring a new swivel, significantly reduces hydraulic restriction by increasing return-flow capacity by 160 percent and by increasing open-flow capacity by 30 percent. Less restriction results in faster cycles and lower fuel burn.

Caterpillar supports its work tools with a comprehensive range of pre- and after-sales services, including advice about selection, operator training, equipment management, and a range of financial and insurance products. For more information about GSH420/GSH520 grapples, contact the local Cat dealer or visit www.cat.com/products.                               

# # #

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Trimble Navigation Limited, registered in the United States and in other countries.

©2018 Caterpillar All Rights Reserved

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests

www.cat.com/requestCatinfo