Caterpillar Introduces Its First Inverter Generator

For Release in the United Kingdom: March 2018 
Release Number: 204PR18

New Cat® INV2000 Offers Professional-Grade Performance in a Consumer Product

Caterpillar is expanding its Home and Outdoor Power product line with the introduction of a portable inverter generator. Inverter technology is a first in Caterpillar’s long history of power generation. Caterpillar engineers designed the Cat® INV2000 with consumer usability features, like an easy start switch, along with professional performance and safety features, making it a versatile generator for both contractor and recreation use. Caterpillar will also offer a parallel kit, enabling users to connect two INV2000 units together, to double power output.


The INV2000 produces 1800 watts rated and 2000 maximum watts-  that’s enough to power camping essentials as well as small to mid-sized power tools (circular saws, etc).  The new generator provides an ultra-clean power (<3 percent total harmonic distortion) that will safely power the most sensitive electronics. Noise levels are competitive in the product category – 59-69 dB (depending on load) – which translates to barely-there white-noise in most environments.

Comfort and Easy Operation

At only 22.2 kg, the INV2000 is easily portable and convenient to store. Intuitive controls, including the easy-start switch with integrated choke, multiple outlets and operational indicator lights, are situated centrally on the front facing panel.  The unique LED illumination of the control panel makes night operation especially convenient.

Along with two 230V 13A outlets, this generator has two built-in USB ports for charging sensitive electronics such as phones, tablets and Bluetooth speakers. The unit also features a 12V battery charging outlet, along with a cable, for easy charging of automotive style batteries. 

Long, Reliable Run-Time

The INV2000 is built with a fuel efficient 79.7 cc overhead valve (OHV) engine, the Engine Smart Control mode adjusts the power output to automatically control fuel consumption and noise based on load, giving users a generous 6 hours of continuous run time on one tank of fuel (at 50% load). 

Simple Maintenance

Caterpillar solved some of the common hassles with inverter generator maintenance with the INV2000 design. Dual access doors (versus a single door) on the side of the inverter provide easy access for basic maintenance procedures such as oil changes, air filter changes and carburetor draining. The custom oil fill design with a threaded oil funnel enables completely dripless oil filling and draining, preventing mess and smoking caused by spills inside the generator.

The INV2000 is CE certified and will be available to purchase from March 2018 at select retailers. Like all other generator models in the Home & Outdoor Power line up, the Cat INV2000 is covered by a full 3-year warranty.

For more information on the inverter and sales locations visit:

# # #

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2018 Caterpillar All Rights Reserved


1 Portable Cat INV2000

Print Media

Placeholder image

Download High Resolution Image

1 Portable Cat INV2000


Placeholder image

Download High Resolution Image

2 Portable Cat INV2000


Placeholder image

Download High Resolution Image

5 Cat INV2000 Easy access


Press Inquiries

Caterpillar Trade Press Media Representatives


Sharon Holling:

Johanna Kelly:

Europe, Africa, Middle East

Francine Shore:

Reader Requests