Caterpillar announces new Cat® M320 Wheel Excavator

The design focuses on operator productivity and reduced downtime.

IRVING, Texas, May 12, 2026 – Customers today are demanding strong machine and jobsite performance that helps lower operating costs and increase productivity. Designed for construction, utility and road maintenance applications, the new Cat® M320 wheel excavator delivers enhanced ease of use, efficiency, stability and reduced operating costs.  

Operator environment and controls

The M320 cab is designed with controls that are easy to reach to help support operator comfort and capability. A high‑resolution touchscreen monitor provides an intuitive interface to help operators maintain consistent performance throughout the workday.

The M320 also incorporates a new auto axle lock feature that automatically activates when the travel pedal is in neutral and the machine speed is near zero. A two-way travel pedal supports machine movement. Compared with the previous model, the M320’s long wheelbase helps improve stability.

 

 

Maintenance and safety

Cat M320 customers can achieve up to 17% lower maintenance costs compared with the previous design, helping reduce downtime and improve overall machine uptime.1


Additional features include:

  • Hydraulic filter features an increased 2,000-hour replacement interval and anti-drain valves
  • Parts commonality with the 320 excavator 
  • Long greasing intervals
  • Small cab pillars and large windows
  • Optional right-side-view cameras
  • In-cab swing lock helps prevent unintentional swing movement and allows the front linkage to be securely locked during machine travel

Increased efficiency

Powered by the Cat C4.4 engine, the M320 meets China Nonroad Stage IV and Brazil MAR‑1 emission standards and emits equivalent to U.S. EPA Tier 3 and EU Stage IIIA. Automatic Engine Speed Control helps reduce fuel consumption by allowing the engine to enter idle mode when the machine is not working. Extended maintenance intervals further support reduced downtime over the life of the machine.

The M320 can travel at speeds up to 35 km/h (22 mph). Its advanced hydraulics system balances power and productivity while providing precise digging control. Auxiliary hydraulic options support a wide range of Cat attachments, with attachment commonality shared with the Cat 320 excavator.

 

More information on the new Cat M320 wheel excavator can be found by contacting a Cat dealer or visiting cat.com.

1 Maintenance costs based on comparison of M320 (04B) and M320 (05D) recommended maintenance interval schedule and recommended component rebuild schedule.

of

Cat® M320 Wheel Excavator working shot.

View Full Size Image
of

Cat® M320 Wheel Excavator maintenance shot.

View Full Size Image
of

Cat® M320 Wheel Excavator with hammer attachment.

View Full Size Image
of

Cat® M320 Wheel Excavator with hammer attachment.

View Full Size Image
of

Cat® M320 Wheel Excavator working shot.

View Full Size Image
of

Cat® M320 Wheel Excavator roading.

View Full Size Image

 

 

Download the Press Release

Download Now

Download the Images 

Download Now

 

 

# # #

 

About Caterpillar:
For more than a century, Caterpillar has helped build a better, more sustainable world. With 2025 sales and revenues of $67.6 billion, Caterpillar Inc. is shaping the future as the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. Backed by one of the largest independent global dealer networks and financing services through Cat Financial, the company’s primary business segments: Power & Energy, Construction Industries and Resource Industries are solving customers’ toughest challenges through commercial excellence and advanced technology, driven by a highly skilled, dedicated global team. Learn more at www.caterpillar.com

Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.

 

 

Press Inquiries:

Johanna Kelly
Caterpillar Trade Press Media Representative
Kelly_Johanna_L@cat.com
 
For Release: Africa, China, Middle East, South America and Southeast Asia 
Release Number: 9PR26 - May 2026


Wheel Excavators

Cat® wheeled excavators have the mobility, speed, power, and reliability to be the most versatile machine in your fleet. They help you take on a variety of challenges every day, and at a lower cost.

Learn More
M320 Wheel Excavators
M320 Wheel Excavators

The Latest Product News

Get the Latest Stories Sent Directly to Your Inbox.

Subscribe Now