See the latest product and engine announcements from Caterpillar.
See the Latest NewsSign In
Welcome! Sign In to personalize your Cat.com experience
If you already have an existing account with another Cat App, you can use the same account to sign in here
Register Now
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Release in South America, Africa, Middle East, Asia: August 2019
Release Number:907PR19
Caterpillar announces the release of 9 new Cat® D3 Series Skid Steer Loader (SSL) and Compact Track Loader (CTL) models. These new machines advance the D Series’ reputation for quality, comfort, and performance and deliver improvements in operator experience, and track loader stability. An industry first, the D3 Series models also support a line of new Smart Attachments. This advanced machine technology recognizes certain attachments and tailors the controls and operator information to match the tool and the task.
Improved Operator Experience
Entering and exiting the new D3 Series loaders equipped with an enclosed cab is now easier thanks to a wider opening cab door. Additionally, the distance between joystick pods has increased by 3 in (76 mm), offering extra space for the operator inside the cab to deliver a more comfortable experience.
Raising Compact Track Loader standards
New Cat D3 Series CTLs deliver improved operating stability while handling heavy loads, grading or truck loading. Changes to the undercarriage frame and torsion axles reduce machine pitching and rocking, while still offering superior ride comfort.
All Cat D3 Series CTLs feature standard two-speed travel to improve performance at the jobsite. These machines are geared to deliver high torque digging performance as well as high top-end speed for travel. The powerful Cat 279D3 and 289D3 loaders boast an 8.4 mph (13.6 kph) top-end ground speed, a 20 percent increase over their D Series counterparts.
Advanced Control
The D3 Series Cat SSL and CTL models deliver Smart Technology that ushers in a higher level of integration between the machine and new Smart Attachments. This advanced attachment technology will allow the D3 Series Cat SSL and CTL models to automatically recognize Smart Attachments and convert machine controls to align with the operational and informational needs of that attachment.
Cat SSLs and CTLs offer advanced control features that include Return-to-Dig and Work Tool Positioner to assist operators with repetitive tasks like grading, digging, and loading. These items are now bundled together with the dual direction self-level feature so that even more operators will be able to take advantage of features that automate machine functions to allow these tasks to be completed with less user interaction and expertise.
For more information on the new Cat D3 Series of SSLs, CTLs, visit your local Cat dealer or www.cat.com.
|
232D3 |
236D3 |
242D3 |
246D3 |
262D3 |
Engine |
Cat C2.2 |
Cat C3.3B |
Cat C3.3B DIT |
Cat C3.3B DIT |
Cat C3.3B DIT |
Gross power, |
60.2 |
74.3 |
74.3 |
74.3 |
74.3 |
Operating weight, |
6,514 |
6,567 |
7,138 |
7,478 |
8,296 |
ROC @ 50%, |
1,900 |
1,800 |
2,200 |
2,200 |
2,700 |
|
257D3 |
259D3 |
279D3 |
289D3 |
Engine |
Cat C3.3B |
Cat C3.3B |
Cat C3.3B DIT |
Cat C3.3B DIT |
Gross power, |
74.3 |
74.3 |
74.3 |
74.3 |
Operating weight, |
8,094 |
8,987 |
10,095 |
10,688 |
ROC @ 50%, |
2,570 |
2,870 |
3,170 |
4,130 |
# # #
Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
VisionLink is a trademark of Trimble Navigation Limited, registered in the United States and in other countries.
©2019 Caterpillar All Rights Reserved
Press Inquiries |
Caterpillar Trade Press Media Representatives Americas Sharon Holling: Holling_Sharon_L@cat.com Johanna Kelly: Kelly_Johanna_L@cat.com Europe, Africa, Middle East Francine Shore: Shore_Francine_M@cat.com |
Reader Requests |
www.cat.com/requestCatinfo |