Solar design strategies: passive versus active

Solar design strategies: passive versus active

This article compares passive versus active solar design strategies and explores the differences between the various types of solar panels.

Two of Page's sustainability experts, Mackenzie Manson and Joanna Yaghooti, recently collaborated on a brief overview of the use of solar energy as part of an overall strategy to conserve resources and promote energy independence. This article compares passive versus active solar design strategies and explores the differences between the various types of solar panels.

 

Passive design

Passive solar is a design strategy focused on the thoughtful design of windows, walls and floors to collect and distribute solar energy in a building. This simple strategy requires little to no mechanical or electrical systems (and no moving parts). Vernacular architecture is well-known for its intuitive use of passive solar design.
Passive solar strategies include orienting the building in response to the sun’s path, shading the building, using materials with favorable thermal-mass properties for the climate, and designing the interior spaces of the building to assist in effectively heating and cooling the building naturally. Passive solar technologies reduce the building’s reliance on mechanical and electrical systems to heat, cool and light the building. It is a foundation on which high performance buildings are conceived.

Active design

Active solar technology uses equipment to convert solar energy into usable electricity or to heat water for process or domestic use in the building. These technologies are steadily evolving and their efficiency is improving rapidly.

Competitive pricing from the fall of 2014 puts a typical roof-mounted installation at approximately $3 to $3.50/W (inclusive of material, labor, inverters, mounting and electrical, but exclusive of incentives and rebates). A typical mid-rise office building (approximately 130,000 gsf) can expect to install an array comprising 154 250w panels for approximately $115,000 (before rebates). Depending on the building’s load profile, a system at this scale can be expected to mitigate up to 6% to 10% of the building’s energy demand. Regional variations can greatly affect production and installation costs.

Passive design considerations

  • Microclimate
  • Taking into consideration that buildings in humid environments require different passive strategies than buildings in an arid climate
  • Building orientation
  • Positioning the long side of a building in a north-south orientation whenever possible
  • Fenestration orientation
  • Sizing and configuring windows to minimize heat loss
  • Shading windows to further minimize heat loss
  • Thermal mass
  • Designing solid walls with thermal properties that follow vernacular rules regarding storage and release of heat.

Active design considerations

  • Designing large, unobstructed roofs or ground areas ideal for photovoltaic panel arrays. Trees, mechanical units and other buildings should not shade the panels at any time.
  • Determining the optimal solar panel installation angle. Panels typically produce the most energy when tilted at an angle equal to the latitude of the sun at that specific location.
  • For buildings with smaller floor plates, installing panels on parking structures or covered parking pavilions.
  • Installing an energy dashboard for tracking and displaying the array’s performance. The energy dashboard also educates the building occupants on how their behaviors impact building performance.

POWER SYSTEMS TRAINING

power systems training

Whether onsite or online, build your business with seminars and webinars from the experts. Get the most out of your equipment with training and support from Caterpillar.

learn more

renewable energy

Microgrids provide value to prime power diesel and gas customers by integrating renewable energy, such as solar power, with generator sets.

View Renewable Energy page