Cat® Utility Vehicle Makes the Grade on Harsh Job Site

All-New Cat CUV82 is put to the test on a high-profile sports center construction project
Watch the Cat CUV82 power through the muddy terrain on the Eagan, MN-based sports center project site, and hear what the Frattalone Companies crew has to say about its performance.

St. Paul, MN-based Frattalone Companies got its start in excavating and grading work in 1970, and has since earned a reputation for delivering the highest quality of work for its customers. The contractor is currently working on a multiyear, multiphase demolition, grading and construction project to develop a new sports center complex in Eagan, MN. The project is no small undertaking, with a job site spanning 200 acres and the development of office spaces, a training facility, two medical facilities, five practice facilities and a 6,000-seat stadium at completion.

Since the project started in in mid-2016, the crew has had to contend with two seasons of nearly constant rain, creating an extremely muddy, difficult work site. In addition to their fleet of construction machines, Frattalone Companies needed a utility vehicle that could navigate through the rough terrain.

“We have been using and testing utility vehicles on large projects for more than five years, and they are a very big part of our fleet,” says Tony Frattalone, president of the company. “If you think about it, it’s more economical to transport people and tools across a site using a $15,000 UTV compared to a $65,000 pickup.”

The particularly harsh conditions of this project presented the perfect opportunity to put the new Cat Utility Vehicle through a rigorous field test. And as a long-standing Caterpillar customer, Frattalone Companies was on board, and ready to put it to work. So the product team worked with Frattalone’s dealer, Ziegler Cat, to deliver a Cat CUV82 Utility Vehicle prototype to the site to see how it would perform in the unforgiving environment.


The Making of the All-New Cat® Utility Vehicles

The Making of the All-New Cat® Utility Vehicles

From initial sketches to rigorous machine testing, the Caterpillar product team brings you an inside look at the design and innovation behind the first-ever Cat UTVs.

Go Behind the Scenes

 

Cat CUV82

With a maximum speed of 45 MPH, a 50 hp engine and 1,000 lb. rear cargo capacity, the gas-powered CUV82 is ready to perform on any work site.

Learn more

Cat CUV102D

Featuring a 1,000 lb. capacity steel cargo bed and 4-wheel independent suspension, the diesel-powered CUV102D is designed for stable load hauling and transport over any terrain.

Learn more


 

Connect with a Cat Dealer

We’ll put you in touch with your local dealer so you can to find out when the Cat Utility Vehicles will arrive at a location near you.