The American Civil War was raging when Captain James “Whiskers” McAllister launched his company in 1864 with a single vessel. One hundred and fifty-six years later, McAllister Towing and Transportation found itself in the midst of another battle — the fight against the COVID-19 pandemic.
On March 30, 2020, four McAllister tugboats, all powered by Cat® engines, escorted the USNS Comfort hospital ship into New York Harbor. It wasn’t the first time the New York-based, family-owned company had turned to Cat engines for a critical maneuver. McAllister has relied on Cat power since the 1960s, and several of its 50-plus vessels are still powered by Cat marine engines that date back to that decade.
Tugboats, which help larger ships maneuver in tight spaces and make small, precise turns to dock safely, need engines that can react quickly to changes in conditions.
“If we’re docking a ship and it starts to move in the wrong direction, we can’t wait 30 seconds or a minute for the engine to power up,” says Marty Costa, McAllister’s engineering manager. “Cat engines have the power and responsiveness we need. In fact, the first time the pilots on the Capt. Brian A. McAllister told us to give it full power, they weren’t prepared for how much the engines had and told us, ‘Whoa, not that much power!’”
One of the company’s newest vessels, the Capt. Brian A. McAllister is among five McAllister tugboats powered by Cat engines that meet U.S. EPA Tier 4 Final emission standards. These Cat engines use a selective catalytic reduction (SCR) aftertreatment system and diesel exhaust fluid (DEF) to reduce NOx emissions to extremely low levels. Other engine manufacturers chose a different path to meet Tier 4 Final regulations, but Costa is pleased with the Caterpillar solution.
“The engines we’ve seen without SCR are very heavy, very big and very slow,” he says. “We haven’t had any trouble with the Cat engines or with DEF supply. They’re cleaner and they get better fuel economy. Any issues we had at the beginning, Caterpillar and the dealer were quick to fix.”
That type of responsiveness from McAllister’s primary Cat dealer, Foley Inc., and the rest of the Cat dealer network is a big reason the company continues to choose Cat engines.
“We have boats up and down the East Coast, and no matter where we are, we can get service,” Costa says. “If there’s a problem, they can have a technician out whenever we need them. We don’t have extra boats sitting on the back burner — if we have two boats in a port, they both have to be working.”
Proactive maintenance is key to keeping McAllister’s tugs on the water and operating reliably. The company handles service for older tugs itself and relies on the Cat dealer network for new vessel maintenance, engine rebuilds and the flexibility to tailor service around its tugboats’ specific needs.
“Caterpillar normally uses hours as the criteria for service intervals, but our tugs spend a lot of time operating at low RPMs, burning lots of fuel,” Costa says.
Though the USNS Comfort docking put McAllister in the media spotlight, it was just another day’s work for one of the oldest, largest towing and transportation companies in the United States.
McAllister plans to keep getting it done with the help of Cat marine power.
Like many great ideas, Caterpillar’s solution to address the latest marine emissions Tier 4 standards started with a simple pencil sketch. Now that design is helping customers reduce emissions and operating costs.
Learn MoreThe Cat 3500 engine series is already one of the most proven engine systems in the world, and it’s getting better with the shift to U.S. EPA Tier 4 Final emission standards. The 3516E model, specifically, is designed for marine operations and offers the best PM and NOx reduction technology, in the form of an improved SCR system. Along with SCR comes an impressive collection of features and options that can be tailored to any marine operation, as well as compliance with essential safety regulations.
Learn MoreTo address the challenge of lower emissions, Bisso Towboat Co. chose Cat® 3516E marine engines for the Andrew S, making it the first tractor tug on the Mississippi River to meet Tier 4 Final standards.
Learn More