Empowering Patient Care

Powering Covid Testing Sites

Cat® power helps hospitals test for COVID-19 safely.

Generators, Fuel Tanks and Tents Are Now Indispensable to Atlanta Hospitals

 

Many hospitals have veered into uncharted territory during the COVID-19 pandemic, requiring them to operate differently to limit virus spread, while also still caring for patients. 

For many Atlanta hospitals, that new way of working now includes tents. Lots of them.

The tents serve as initial screening locations, intentionally located away from the hospital to limit exposure for those who aren’t infected. People who tested positive for COVID-19 are admitted to the hospital, while non-infectious patients are either treated on-site or sent to a safe location for further evaluation and treatment.

Powering Hospital Tents with Generators

However, this isn’t your typical camping or tailgating tent set up; these tents need plenty of power for lights, medical equipment and AC to ensure patients and staff are both safe and comfortable.

For Cat® Dealer Yancey Power Systems, it’s been an opportunity to step up and help local hospitals adapt to a new way of working.

From the very beginning, the Yancey team considered every detail of the medical tent set up: the exact equipment and generators required, the equipment set up as well as the type of generator power required to ensure the sites could stay up and running without interruption.

Simplifying Hospital Equipment Needs

“In our walk-throughs of each site, we designated where all of the equipment needed to go, keeping in mind that they’ll need to run this for about two months,” said Peter Moore, a healthcare account manager for Yancey Power Systems. “We pointed out that if they are going to run 24 hours a day for that period of time, the generators will need to be serviced. So, we also developed a plan so we can access all the units and pull them out and service them.”

To simplify the set-up process, Yancey partnered with an additional vendor so that each tent (including the Cat generator, equipment, fuel tanks and more) could be sent to hospital facilities staff as a complete package.

Putting the Community First

The tent coordination was a little extra work up front, but well worth the effort to help the already-burdened hospital teams.

“It’s about taking care of the customer, and that’s ingrained in our culture. It’s really about follow-up, follow through, and truly caring during this time when lives are on the line,” said Drew Eckford, Yancey Rental Power manager.


“IT’S REALLY ABOUT FOLLOW-UP, FOLLOW THROUGH, AND TRULY CARING DURING THIS TIME WHEN LIVES ARE ON THE LINE.”

 

Providing hospital power is nothing new for the Yancey team.  But this project was about more than power, it was about community.

“We’re all in this together—any of us could be affected at any moment. There are a lot of people that would avoid even the thought of going around a hospital right now, and our Yancey team is out there servicing these locations in order to make sure that we can help our community in a time of absolute need.”

Learn more about Power System Rentals and Cat Electric Power

Yancy Power Systems
of

The Yancey Power Systems team set up a Cat® XQ125 mobile generator set to feed a 12-ton AC unit, along with a 75kVA transformer connected to a splitter with GFCI outlet that provides multiple connection points around the tent.

Covid-19 Testing set up outside
of

Screening tents were set up outside the hospitals and were fully equipped with air conditioning and power for medical equipment.

Generator
of

The Yancey team planned the entire set up so that equipment could be easily serviced without interruption to the medical staff.

Yancy Power Systems
Covid-19 Testing set up outside
Generator

GET STORIES, PLUS THE LATEST NEWS, DELIVERED TO YOUR INBOX

Sign up for our monthly newsletter to stay up-to-speed on all things Cat, including helpful tips to grow your business. Expect industry updates, exclusive offers and more to help you do the work.

Sign Up
eNews Signup

Related Stories