Caterpillar Marine Offers More Horsepower with C32B 2433 MHP Engine
Houston, Texas – Following the successful launch of the C32B 2025 MHP engine, Caterpillar Marine has announced the release of the new Cat® C32B Triple Turbo 2433 MHP (2400BHP) high-performance marine engine, with a rated engine speed of 2300 rpm. With an incredible 20% increase in power output, the C32B Triple Turbo engine leverages the same core engine upgrades as the C32B 2025 MHP rating while offering additional features and benefits. The C32B 3-Turbo is ideal for yachting, sportfishing, and governmental applications.
Compared to the C32B 2025 MHP model, the new engine has an updated cooling system and a new sequential (3-turbo) air system that delivers faster response and better performance. Additional options include extended oil change intervals, full MCS certification, including duplex filtration, and a cosmetic engine cover.
“We are extremely excited to build on our recent introduction of the C32B by bringing even more power density to the industry with our best-in-class V12 engine. The C32B Triple Turbo engine will be a difference-maker for the high-performance marine segment, both in power and performance. We’re thrilled to work with our customers, dealers, and builders to deliver this outstanding product.” says Allen Bowman, Caterpillar Marine Product Strategy Lead for C32.
The C32B Triple Turbo engine has something to offer for everyone in the high-performance segment, such as higher vessel speed for sport fishers, more environmentally friendly options (IMO III SCR) for motor yachts, and 2025 MHP Intermittent Duty classification for governmental applications. The C32B was designed with repowers in mind to provide more power and life to existing vessels.
The new C32B Triple Turbo complies with EPA Tier 3 Recreational and IMO II emissions regulations, and a fully integrated SCR solution for IMO III. Additional certifications may also be available; please check with your Cat dealer.
The Cat C32B Triple Turbo engine will be available to order in late 2021 and comes with industry-leading warranty coverage. Caterpillar is committed to providing customers with excellent service for the life of their products. Customers can expect the benefits of hassle-free ownership and maintenance, peace of mind from equipment health management, and support from expert dealers a part of the global Cat dealer network.
About Caterpillar Marine:
Caterpillar Marine, with headquarters in Houston, Texas, groups all the marketing and service activities for Cat® and MaK marine diesel, dual fuel, and gas power systems within Caterpillar Inc. The organization provides premier power solutions in the medium and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100 ekW in marine generator sets. The sales and service network includes more than 2,100 dealer locations worldwide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.
More information is available at: www.cat.com/marine
About Caterpillar
Since 1925, Caterpillar Inc. has been helping our customers build a better world – making sustainable progress possible and driving positive change on every continent. With 2019 sales and revenues of $53.8 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. Services offered throughout the product life cycle, cutting-edge technology and decades of product expertise set Caterpillar apart, providing exceptional value to help our customers succeed. The company principally operates through three primary segments - Construction Industries, Resource Industries and Energy & Transportation - and provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect on social media, visit caterpillar.com/social-media.
© 2021 Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, "Caterpillar Corporate Yellow", the "Power Edge" and Cat “Modern Hex” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
Trade Press Inquiries
Danielle Wills