New Cat® C3.6 Offers More Efficiency and Drivability in a Compact, Easy-To-Install Package

New Cat® C3.6 Offers More Efficiency and Drivability in a Compact, Easy-To-Install Package

For Worldwide Release: November 2019
Release Number: 848PR19

Caterpillar Industrial Power Systems is pleased to announce the availability of the Cat® C3.6 industrial diesel engine. The powerful 134 hp (100 kW) engine meets EU Stage V / U.S. EPA Tier 4 Final nonroad emission standards and features 406 lb.-ft of torque at 1500 rpm (550 Nm at 1500 rpm).

With its smaller package and compact design, the C3.6 helps original equipment manufacturers (OEMs) save significant powertrain installation costs while still providing 5% increase in power density and 12% increase in torque than its predecessor engine, the C3.4. That’s because the new engine’s smaller package features flexible aftertreatment solutions that provide original equipment manufacturers (OEMs) with a simplified installation process that also reduces integration costs.

“We wanted to create an engine with customizable aftertreatment that allows OEMs to minimize installation costs while also providing maximum efficiency from the engine,” said Caterpillar product marketing manager Alex Eden. “Technology features such as controllable turbocharging have made it possible to create a smaller engine with the response that would be expected from a much larger product. The torque at low speed, which is critical for machine drivability, is particularly impressive.”

Customers will enjoy the benefits of lower owning and operating costs with the C3.6 thanks to an overall decrease in fluid consumption, including a 6-10% decrease in diesel exhaust fluid (DEF) consumption when compared to the C3.4.

The C3.6 is also backed by the Cat dealer network that is focused on providing world-class service and support for its customers.

“Our dealers take great pride in providing customers the solutions they require,” said Brian Tomsovic, global dealer operations manager. “The dealers are dedicated to truly understanding the challenges OEMs and customers face and creating solutions that meet or exceed their expectations requires a high level of expertise.”

The Cat 3.6 dual-certified, engine is distributed, sold and supported through the worldwide Cat dealer network with trained technicians to ensure service support is never out of reach. To learn more about the C3.6, please visit cat.com.

 

# # #

 

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2019 Caterpillar. All Rights Reserved.

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests
www.cat.com/requestCatinfo

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News