New Cat® Fluid End Design Extends Block Life By 50%

Houston, Texas – By eliminating one of the most common causes of fluid end failure — fatigue cracking at the intersection of the bores — new Cat® Cube Bore well stimulation technology extends block life by 50 percent or more. Available exclusively from Caterpillar, this innovative geometry significantly reduces the downtime and costs associated with fluid end replacement.

“Fluid ends are costly consumable items, and when they reach the end of their lives, it can be a labor- and time-consuming process to replace them,” said Shaun Boller, Caterpillar Oil & Gas pressure pumping specialist. “As the manufacturer, anything we can do to extend the life of the block keeps our customers pumping and earning money.”

What sets Cat Cube Bore apart from other fluid ends is its geometry. Traditional products focus stress to the corners of the intersecting bore, resulting in high concentrated stresses in localized areas. Stress combined with corrosion pitting causes cracks to initiate and spread, compromising the pump’s overall function and leading to block failure.

“We explored a number of ways to solve the problems of stress and cracking,” Boller said. “Ultimately, it came down to one thing — to prevent cracking, you have to eliminate high-stress areas, and that requires modifying the geometry of the fluid end.”

The Cat Cube Bore design disperses stress from the high-pressure bore into the surrounding material. It removes material in critical areas near the bore intersections and smoothes large corners, which in turn smoothes the stress profiles and allows energy to be absorbed by the surrounding block material.

According to validation testing performed in the field, the design completely eliminates the failure mode for intersecting bore corrosion fatigue cracking. Field trials are underway or complete at nine different customer sites across the United States.

“In Cat Cube Bore field trials completed so far, we’ve seen an average increase in durability of 109 percent compared to current production fluid ends,” Boller said. “That’s more than double our original estimate.”

Available to order beginning June 12, 2018, through the Cat dealer network, Cat Cube Bore well stimulation technology works with all current Cat power end and fluid end components. There’s no need for customers to change parts inventory or existing operating and maintenance practices to realize the benefits of extended life and reduced operating costs.

 

Alt Alt
Available exclusively from Caterpillar, Cat® Cube Bore well stimulation technology extends fluid end block life by 50 percent, reducing downtime and costs associated with fluid end replacement.

About Caterpillar Oil & Gas:

Caterpillar Oil & Gas, Caterpillar Inc.’s oil and gas division with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW.  The sales and service network includes more than 2,100 dealer locations worldwide dedicated to supporting customers in the drilling, production, well service and gas compression segments. More information is available at: cat.com/oilandgas

About Caterpillar:

For more than 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2017 sales and revenues of $45.462 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three primary segments — Construction Industries, Resource Industries and Energy & Transportation — and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

 

GET THE LATEST STORIES AND TIPS FROM CATERPILLAR – SIGN UP FOR OUR E-NEWSLETTER

 

 


The new Cat Cube Bore Design for Fluid Ends

The new Cat Cube Bore Design for Fluid Ends

How are fluid ends with the Cat® Cube Bore design performing in real-world situations? Check out the impressive results from our field trials.

Read More

Request More Information

Request More Information

Get the details on how innovative Cat® Cube Bore geometry solves the problem of fatigue cracking to extend life expectancy and lower your costs.

Get Connected

###

 

Press Inquiries – Caterpillar Oil & Gas Press Relations:

Jenna Janik Marcoux
Tel: +1.713.895.1449
Marcoux_Jenna_J@cat.com