Cat® COMMAND for Compaction Helps Contractors Achieve Compaction Quality

For Release in North America: September 2019
Release Number: 744PR19

Caterpillar announces the release of Cat® COMMAND for Compaction, an operator-assisted technology that automates the soil compaction process and helps contractors achieve compaction quality. The COMMAND for Compaction system is available for use on select Cat vibratory soil compactors as a dealer installed kit on both new and existing B-Series machines.

Simple Set-up and Operation

An in-cab display with an intuitive, touchscreen interface makes setup easy and the system connects to common base stations with no back office or design needed. The operator uses the machine to map the boundaries of the area to be compacted and enters the compaction parameters. Once the operator places the machine in “auto,” the system will control the propulsion, steering and vibration of the machine. Recent jobs are saved in the system and can be accessed through the touchscreen interface.

An integrated object detection system alerts the operator if an object is in the pathway.  If there is an area that cannot be compacted using vibration, the operator can choose to turn the vibration system off and give control back to the system once the area has been passed.

Consistent Results

By automating the compaction process, operator skill gaps are minimized by providing consistent results based on operator inputs. COMMAND for Compaction enables compaction quality by maintaining constant speed and correct pass count with consistent and precise overlap, allowing contractors to hit compaction targets more frequently.

Cat COMMAND for Compaction will be available in first quarter 2020. For more information, contact your local Cat dealer.

# # #

 

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2019 Caterpillar All Rights Reserved 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests
www.cat.com/requestCatinfo

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News