Caterpillar brings intelligent solutions to life at CONEXPO-CON/AGG 2026
At CONEXPO‑CON/AGG 2026, Caterpillar is showcasing a broad spectrum of intelligent solutions designed to address those challenges now, with technology that works on real jobsites and integrates with how customers already operate.
Highlights
- Connecting customers’ entire fleet of equipment: VisionLink™ expands to support on-highway assets with added safety features for all equipment
- Intelligence on the jobsite: Cat® AI AssistantTM launches with personalized insights and recommendations in digital apps; in-cab prototype on display at show
- From Cat AI Assistant to autonomy: a broad spectrum of solutions that meet customers where they are
LAS VEGAS, March 1, 2026 – Construction’s toughest challenges — a persistent labor shortage, rising safety demands and the pressure to do more with less — are driving a fundamental shift in how jobsites operate. At CONEXPO‑CON/AGG 2026, Caterpillar is showcasing a broad spectrum of intelligent solutions designed to address those challenges now, with technology that works on real jobsites and integrates with how customers already operate.
The connected operation: One platform for the full fleet
VisionLink™ is the flagship application of Caterpillar’s technology portfolio — unifying fleet data and operational analytics to deliver actionable insights. It’s where customers maximize the value of their assets and technology investments. With data from approximately 1.6 million connected assets in the field built on Caterpillar’s equipment expertise, the platform grows smarter as more assets come online.
The need for asset visibility doesn’t stop at Caterpillar iron. Customers today run a variety of assets in their fleets – from pickup trucks to concrete mixers to dozers.
Among the latest VisionLink updates featured at CONEXPO-CON/AGG:
- Full fleet management capabilities through a new relationship with Geotab Inc. that unlocks on-highway assets for a single view of customers’ entire fleet.
- Enhanced safety monitoring that tracks leading indicators like machine overspeed events and seat belt usage, giving customers visibility to identify and address high-risk conditions before incidents occur.
- Integrated video playback enables event review to improve customer awareness and training in real‑world circumstances.
Cat® AI Assistant™
Caterpillar’s new AI solution will deliver value to customers in new, powerful ways. The Cat® AI Assistant™ is an easier way for customers to buy, maintain, manage and operate their equipment – on and off the jobsite. It draws from Caterpillar data, including connected assets, operation and maintenance manuals, parts catalogs, purchase history and more, to provide personalized insights and recommendations.
Featured at CONEXPO-CON/AGG:
- Cat AI Assistant is now available out of the cab, helping customers on existing Cat® platforms and applications.
- An in-cab Cat AI Assistant prototype is showcased, marking a major step forward for Industrial AI.
Ogi Redzic
Chief Digital Officer
Caterpillar
Intelligence delivered: AI, autonomy, and precision on the jobsite
For an operator, the Cat AI Assistant in-cab will connect throughout the workday — from machine startup to shift handoff. It will act as a coach when prompted, providing operators with information to work smarter and safer without switching screens, returning to the yard or losing focus. The Cat AI Assistant leverages NVIDIA’s platform to run speech recognition and advanced AI models will assist with directing the machine.
Collision Mitigation
On jobsites, blind spots behind machines remain one of the most persistent safety risks. Caterpillar’s new Collision Mitigation System is an operator-assist feature designed to address that challenge directly. Using an integrated sensor array, the system enhances situational awareness when reversing by detecting people and obstacles across three proximity-based zones behind the machine.
Beyond visual and audible alerts, the system can inhibit machine motion and enable automatic emergency braking, actively intervening to help reduce struck-by incidents. Event data, safety trends, and video playback feed into VisionLink, giving managers visibility into jobsite risk patterns over time.
Cat Grade precision automation
Cat Grade delivers accurate, consistent grading using advanced sensors and automated controls for both 2D and 3D applications, reducing the need for manual staking and survey crews. Cat Grade works with Trimble, Topcon and Leica systems and can be installed on other machine brands. Available for dozers, excavators and motor graders, Cat Grade integrates with VisionLink to enable remote file delivery, drone survey integration and productivity tracking.
From Assist to autonomy: Proven technology that works
Caterpillar has been a pioneer in autonomy for more than thirty years, starting in mining where remote and hazardous environments demanded innovative approaches to safety and productivity. Today, that expertise spans a broad spectrum: on-machine assist and detection features that build operator confidence, remote and semi-autonomous operations through Cat Command, and coordinated autonomous tasks with site-level supervision.
Jaime Mineart
Chief Technology Officer
Caterpillar
Expanded Cat Command capabilities
For customers looking to keep operators out of hazardous conditions while maintaining full control of the work, Cat Command allows operators to control heavy equipment from a safe distance using either line-of-sight or non-line-of-sight controls. The system includes semi-autonomous functions like auto-dig, auto-dump and automated grading. It now covers an expanded range of equipment, with capabilities from remote control through semi-autonomous and autonomous-ready functions for wheel loaders and dozers.
Caterpillar provides multiple entry points for technology adoption—ranging from safety and operator-assist solutions powered by VisionLink and the Cat AI Assistant to remote and semi-autonomous capabilities, extending to fully autonomous operations. Every solution is designed to seamlessly build on customers’ existing equipment and systems.
At CONEXPO-CON/AGG, attendees will see what that looks like in practice. Inside Caterpillar's Performance Center in Operator Stadium, a customer will operate two Cat 938 wheel loaders located in Naples and Punta Gorda, Florida, from the show floor. A Command Station will also let attendees remotely operate a Cat 745 articulated truck, part of the most complete Command portfolio ever shown for Construction Industries. And in Operator Stadium, semi-autonomous compaction will be running live on the Cat CS12 single drum roller.
From productivity gains to safer operations, Caterpillar technology delivers real jobsite value—helping customers operate more efficiently and solve their toughest challenges. Every solution on display at CONEXPO‑CON/AGG is designed to meet customers where they are, work with what they already have, and build toward what’s next.
More information on advanced Cat technologies can be found by visiting a Cat dealer or cat.com.
# # #
About Caterpillar:
For more than a century, Caterpillar has helped build a better, more sustainable world. With 2025 sales and revenues of $67.6 billion, Caterpillar Inc. is shaping the future as the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. Backed by one of the largest independent global dealer networks and financing services through Cat Financial, the company’s primary business segments: Power & Energy, Construction Industries and Resource Industries are solving customers’ toughest challenges through commercial excellence and advanced technology, driven by a highly skilled, dedicated global team. Learn more at www.caterpillar.com.
Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.
Press Inquiries:
Kate Kenny
Caterpillar Trade Press Manager
Kenny_Kate@cat.com
For Release: Worldwide
Release Number: 40PR26 — March 2026
The Latest Product News
-
New Cat® D11 Xe Electric Drive Dozer Delivers More Productivity and Lower Operating Costs
Cat® D11 XE electric drive dozer helps mining operations move more material with improved fuel efficiency and lower operating costs through an electric drivetrain designed for productivity and simplified service.
Learn More -
BHP, Rio Tinto and Caterpillar launch battery-electric haul truck trial in the Pilbara
BHP, Rio Tinto and Caterpillar have launched a trial of two Cat® 793 XE Early Learner battery-electric haul trucks at a mine-site demonstration in Western Australia’s Pilbara as part of an industry-first collaboration.
Learn More -
Carmeuse Selects Caterpillar’s Autonomous Hauling Solution to Deploy at Drummond Island Operation
Caterpillar Inc. today announced an agreement with Carmeuse, a global leader in lime and limestone production, to deploy Caterpillar’s autonomous hauling solution at the Carmeuse Drummond Island quarry in Drummond, Michigan.
Learn More -
New Cat® 6040 mining shovel helps mining operations improve productivity and efficiency
The new 400-tonne-class Cat® 6040 next generation hydraulic mining shovel is designed to help customers address these challenges through productivity enhancing features, durability upgrades and system improvements that increase efficiency.
Learn More