Caterpillar presents broad range of new machines and capabilities at bauma CHINA 2018

Caterpillar presents broad range of new machines and capabilities at bauma CHINA 2018

For Worldwide Release: October 2018 
Release Number: 534PR18

Caterpillar will display 30 machines as well as work tools, engines and product support capabilities at bauma CHINA 2018. The extensive exhibit will feature Cat® general construction, building construction, paving and SEM-branded equipment. More than a dozen Cat Next Generation hydraulic excavators will be introduced at the show.

Caterpillar’s indoor display will occupy more than 3 000 m2 of prominent space in the N1 exhibit hall. In addition, Caterpillar will present outdoor demonstrations (booth A60, 1 144 m2) that will offer visitors opportunity to experience first-hand the capabilities of Cat machines, work tools and technologies. 

General Construction

Cat earthmoving machines at bauma CHINA 2018 will include 11 hydraulic excavator models, with both wheel and track undercarriages, ranging from the 313D2—with a maximum operating weight of 14 600 kg (32,000 lb.) —to the 390F L, having a maximum operating weight of 96 275 kg (192,680 lb.). Seven machines—330, 330 GC, 336, 336 GC, 345 GC, 320 and 323—are Cat Next Generation models, featuring significant technology advances, including reductions in fuel consumption of as much as 15 percent in some applications, and up to 25 percent for the 320 and 323.

For loading and hauling contractors, Caterpillar will display a Cat 772 off-highway truck, with a rated capacity of 31.3 m3 (41 yd3) and a gross power rating of 446 kW (598 hp). The truck will be paired with the Cat 986K wheel loader, which has bucket capacities ranging from 5 to 10 m3 (6.5 to 13.5 yd3).

The display will include three additional wheel loaders —the 950 GC, 980L, and 982M —as well as the 140 GC motor grader. The motor grader features a new, ergonomically designed cab with an adjustable control console, and it delivers as much as a 10-percent reduction in fuel consumption when the new ECO Mode is used.

An outdoor demonstration will feature the Next Generation 320 and 323 excavators, which use an estimated 25 percent less fuel than predecessor models in certain applications. A new Smart Mode automatically matches engine and hydraulic power to specific digging conditions, and an advanced hydraulic system is designed to balance power and efficiency with precise control. A standard grade-control system, Cat GRADE with 2D, includes both indicate-only and laser capability, and an available suite of Cat Connect Technologies is designed to increase operator efficiency, reduce operator fatigue, and reduce overall operating costs

Building Construction

Cat building construction machines will include six Next Generation mini-excavators—301.5, 301.7 CR, 302 CR, 307.5, 308.5, and 310—as well as a 246 skid steer loader with multiple work tools. The new Next Generation excavators are designed for productive performance and optimum operator comfort, while reducing fuel consumption and overall operating costs. An additional outdoor display will feature a Next Generation model at work to demonstrate the versatile capabilities of these new models.

Cat building construction products are designed and manufactured to meet customer requirements for performance and reliability while delivering high value in the form of durable structures, low fuel consumption and extended service intervals. Cat building construction products are designed to deliver best-in-class digging, lifting, and multifunction capability, including auxiliary hydraulic systems that expand the range of compatible work tools. Caterpillar design provides features that enhance operator productivity, such as adjustable hydraulic response rates. Design experience also ensures fast, uncomplicated routine service.

Paving

Paving products at bauma CHINA 2018 will include the PM620, a high-production, highly maneuverable, half-lane milling machine that can perform controlled, full-depth removal of asphalt and concrete pavements in a single pass; the CS79B soil compactor that features a pod-style vibratory system that is virtually maintenance free, with the first scheduled maintenance period at 3 years or 3,000 hours; and the CB1.7 utility compactor, a dual-drum, 1.7-ton-class roller with a 39-inch-wide drum with a double bevel, making this utilitarian machine suitable for the rental market and for applications such as bike paths, patch work, parking lots, driveways, and shoulder work.

SEM Equipment

Shandong Engineering Machinery Co. Ltd. manufactured SEM-branded wheel loaders in China for more than 50 years and became a Caterpillar subsidiary—Caterpillar (Qingzhou) Ltd. — in 2008. The SEM line now includes small- and mid-sized wheel loaders, 18- to 22-ton soil compactors, mid-size motor graders and dozers. The machines are designed for customers in domestic Chinese markets and for select growth markets around the world.

SEM products at bauma CHINA 2018 include the new 680D wheel loader, which features transmission with electronic clutch proportional control valve with single clutch speed shift strategy to provide higher shift quality; the upgraded 162 kW (220 hp) 822D dozer, which features electronically controlled hydrostatic drive; the new MG918 motor grader with loading sensing hydraulic system which features easy operation and lower fuel consumption; and the SCOM522 soil compactor, which features a pod style eccentric design that can extend system life by 50 percent and reduce the maintenance cost as well.

For more information about Cat equipment, contact the local Cat dealer or go to: www.cat.com

 

# # #

Note to Editors: Caterpillar rolls out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.

CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2018 Caterpillar All Rights Reserved 

 

Press Inquiries

Caterpillar Trade Press Media Representatives

Americas

Sharon Holling: Holling_Sharon_L@cat.com

Johanna Kelly: Kelly_Johanna_L@cat.com

Europe, Africa, Middle East

Francine Shore: Shore_Francine_M@cat.com

Reader Requests
www.cat.com/requestCatinfo

Product & Service News

See the latest product and engine announcements from Caterpillar.

See the Latest News