A friend in need

Preparing for Hurricane Maria

Puerto Rico’s leading importer and distributor of high-end spirits, Mendez & Company is a fourth-generation company with a network of four warehouses and approximately $20 million in inventory. It also imports and supplies groceries and other foodstuffs throughout the island. Their warehouses run 24/7 in a temperature-controlled environment, so a constant source of power is critical.

Dire warnings as Hurricane Maria approached prompted Mendez to secure a backup generator to support its own standby power at a refrigerated warehouse facility. Rimco Cat was able to provide an 800 kW generator set in advance of the storm.

 

“They helped us select the best backup generator for our facility, and they helped us install the system,” said facility manager Eduardo Molina. “They helped us keep the generator running during the entire emergency, included special holidays in the middle of the crisis. During that entire time, they were right there with us.”

“When the hurricane hit, we inspected all of our facilities and everything was okay. Our operations continued to work as planned. The backup rental generator from Rimco Cat helped us make that happen along with the technical support and maintenance service they provided to us,” Collazo said.

 


Cat® Mobile Generator Sets

Cat® Mobile Generator Sets

Cat® Mobile Generator Sets are designed to be easily transported around project sites safely and efficiently. A smaller footprint saves space and provides installation versatility on worksites, while a galvanized enclosure is resilient to potentially harsh environments.

See Our Models

Taking a hard look at how much power is enough

Marpor Corporation’s Denny’s restaurants in Puerto Rico had enough Cat standby power to keep their power on through hurricane Maria and to help out their community by handing out 4,000 breakfasts to people in need.

Link to story

Ensuring continuous power

Pharmaceutical company Neolpharma Puerto Rico maintains its own standby power generation system but stood to lose a substantial amount of inventory when Hurricane Maria devastated the island. To ensure continuous power, they rented a Cat XQ 2000 generator set.

Link to story

Cat® dealer shows what it takes to keep the power on

Immediately after Maria hit, Rimco Cat sent two technicians to assist with the operation and maintenance of Auxilio Mutuo hospital’s standby gensets for the duration of the devastating aftermath.

Link to story

Cat® dealer takes on the longest blackout in U.S. history

Three months after the longest blackout in U.S. history, nearly half of the island’s residents remained without power from the utility grid. Caterpillar, the Cat® dealer network, and RIMCO responded in force when Category 5 hurricane Maria caused complete failure of the power grid in Puerto Rico.

Learn More