Cat® Motor Graders move 150 and 160 to the Next Generation platform
Next Generation 150 and 160 graders combine proven power with smarter controls and a full redesigned cab.
Highlights
- Machines receive the redesigned next generation cabs
- Joystick and lever options available
- Increases in power, efficiency and control
LAS VEGAS, March 1, 2026 – Caterpillar continues to shift its range of motor graders to the Next Generation platform, announcing the Cat® 150 and 160 Motor Graders as the latest models to receive the redesign - helping customers solve their toughest challenges through smarter controls, improved efficiency and enhanced operator comfort.
Joystick controls redefine operator comfort
Both models now feature Caterpillar’s easy-to-use joystick steering controls: optional on the Cat 150 and fitted as standard to the Cat 160.
Eric Kohout
Senior Product Consultant for Motor Graders
Caterpillar
Precision grading through smarter power and transmission
The joysticks place transmission, gear shifting and machine-direction control on the left, while the right handles drawbar, circle and moldboard functions as well as throttle control and the manual differential lock and unlock.
Both the 150 and 160 offer exacting control through nine forward and six reverse gears, with a new offering of a finish gear that allows the operator to achieve precise grading results. Used for the final stage of the grading process, the finish gear ensures that the ground is uniform and even, delivering the specified slope and elevation requirements for the most demanding construction projects. The 150 sports a 12-foot moldboard as standard, with a 14-footer on the 160; upgrades are available to 14 and 16 feet, respectively.
Eric Kohout
Senior Product Consultant for Motor Graders
Caterpillar
Redesigned cab enhances visibility and operator experience
“Another obvious improvement is in the fully redesigned cab, first seen on the upgraded 120 and 140 models. Larger windows provide better visibility all around the cab, with particular focus on the moldboard and tires, while we continue the ‘operator first’ approach by improving HVAC and seat adjustment options.”
Integrated technology for safer, faster grading
Visibility can be further enhanced by specifying the optional integrated rear vision, front vision, 360-degree cameras and Caterpillar’s People Detection system, all feeding into the cab’s 10-inch touchscreen. The same touchscreen also controls optional technologies, such as Cat Grade. Both models allow easy upgrades to attachments, ensuring they hit grade faster.
Eric Kohout
Senior Product Consultant for Motor Graders
Caterpillar
The Cat 150 with joystick option will launch in European countries in the second half of 2026. Full launch for all configurations and regions will follow.
More information on the Cat 150 and 160 Motor Graders can be found by contacting a Cat dealer or visiting cat.com
|
150 Joystick |
160 |
Operating weight, kg (lb) |
19 688 (43,361) |
19 853 (43,768) |
Engine power, kW (hp) |
195 (261) |
206 (276) |
Moldboard, ft |
12 |
14 |
# # #
About Caterpillar:
For more than a century, Caterpillar has helped build a better, more sustainable world. With 2025 sales and revenues of $67.6 billion, Caterpillar Inc. is shaping the future as the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. Backed by one of the largest independent global dealer networks and financing services through Cat Financial, the company’s primary business segments: Power & Energy, Construction Industries and Resource Industries are solving customers’ toughest challenges through commercial excellence and advanced technology, driven by a highly skilled, dedicated global team. Learn more at www.caterpillar.com.
Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.
Press Inquiries:
Amy Doughty
Caterpillar Trade Press Media Representative
Amy.Doughty@cat.com
For Release: Worldwide
Release Number: 24PR26 — March 2026
The Latest Product News
-
New Cat® D11 Xe Electric Drive Dozer Delivers More Productivity and Lower Operating Costs
Cat® D11 XE electric drive dozer helps mining operations move more material with improved fuel efficiency and lower operating costs through an electric drivetrain designed for productivity and simplified service.
Learn More -
BHP, Rio Tinto and Caterpillar launch battery-electric haul truck trial in the Pilbara
BHP, Rio Tinto and Caterpillar have launched a trial of two Cat® 793 XE Early Learner battery-electric haul trucks at a mine-site demonstration in Western Australia’s Pilbara as part of an industry-first collaboration.
Learn More -
Caterpillar announces new Cat® M320 Wheel Excavator
The new Cat® M320 wheel excavator delivers enhanced ease of use, efficiency, stability and reduced operating costs.
Learn More -
Carmeuse Selects Caterpillar’s Autonomous Hauling Solution to Deploy at Drummond Island Operation
Caterpillar Inc. today announced an agreement with Carmeuse, a global leader in lime and limestone production, to deploy Caterpillar’s autonomous hauling solution at the Carmeuse Drummond Island quarry in Drummond, Michigan.
Learn More