Caterpillar launches the new Cat® 707 wide body truck with a rebuildable, cost-effective design
With its 66-tonne maximum payload, the versatile new wide body truck design offers the option of standard or heavy-duty configurations and the choice of 40- or 42-m3 sizes to match the material and jobsite conditions.
Highlights
- Rugged durability with integrated Cat® powertrain that is built to be rebuilt
- Ideal pass match with Cat large excavators and wheel loaders
- First model in new product family that broadens Caterpillar’s hauling portfolio
IRVING, Texas, January 30, 2026 – Built for long life and high uptime availability, the durable new Cat® 707 wide body truck features a fully integrated Cat powertrain, including a Cat C13 engine, Cat automatic transmission and proprietary Cat axles. With its 66-tonne maximum payload, the versatile new wide body truck design offers the option of standard or heavy-duty configurations and the choice of 40- or 42-m3 sizes to match the material and jobsite conditions.
We have engineered our new wide body truck with a unique philosophy – it’s built to be rebuilt, offering consistent mechanical availability and longevity through a second lifecycle, which can help lower operating costs.
With its foundation of reliable operation and a cost-effective rebuild option, the new 707 wide body has been engineered, manufactured and field-tested using the latest technologies to ensure the truck is ready for work. This is the first Cat wide body truck model in a new product family that broadens the Cat hauling systems portfolio.
Angel Gonzalez
Global Product Specialist
Caterpillar
Durable performance
The 707 can be configured with the 400-kW Cat C13B engine to meet China Nonroad Stage IV emissions standards or the 358-kW C13, which emits equivalent to U.S. EPA Tier 3. Both options include a standard engine brake set at a high rating. The truck’s six-speed automatic transmission can be equipped with an optional integrated hydraulic retarder. For reliability, the 707 features proprietary Cat axles, integrated Cat powertrain controllers, and Cat wiring and electric harnesses.
Three brake and retardation levels – integrated Cat engine brake, optional Cat hydraulic retarder, and parking and service brakes – provide superior downhill loaded control for enhanced safety and faster hauling cycles. The new 707 offers ideal pass matches with Cat 986, 988 and 988 XE loaders and Cat 350, 374 and 395 excavators for improved productivity.
The new wide body truck’s left-side operator seat placement and optional right-side instructor seat provide easier operation and comfort for the operator and trainer. The cab features sturdy, four-point mounting and protection is provided by a standard falling object protective structure (FOPS) and optional rollover protective structure (ROPS) for enhanced safety. An available reversing camera helps improve maneuvering safety. Automatic shifting with simple gear selection transmission controls helps to increase efficiency, and the truck’s hoist system offers fast, 20-second raise and lower cycle times to quickly unload material.
Low lifecycle costs
The fully integrated Cat powertrain components are mounted to a durable, reinforced chassis. When coupled with flexible Cat Customer Value Agreements (CVAs), customers can achieve higher uptime during the new truck’s service life, while maintaining reliable mechanical performance and longevity through a second lifecycle.
Shutting down the truck safely, a ground-level engine shut-off switch stops fuel to the engine when activated. Grouped service points help customers spend less time and money on maintenance. The new 707 wide body truck offers parts commonality with other Cat machines with common C13 engine, CX31RT transmission and common cab. LED lights provide longer life and brighter illumination with less power consumption and are more resistant to vibration and water damage.
The new Cat 707 wide body truck is available for select regions with U.S. EPA Tier 3 equivalent and China Nonroad Stage IV emissions standards. Companies can contact their Cat dealer for truck availability in the region.
More information on the new Cat 707 wide body truck can be found by contacting a Cat dealer or visiting cat.com.
# # #
About Caterpillar:
For more than a century, Caterpillar has helped build a better, more sustainable world. With 2025 sales and revenues of $67.6 billion, Caterpillar Inc. is shaping the future as the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. Backed by one of the largest independent global dealer networks and financing services through Cat Financial, the company’s primary business segments: Power & Energy, Construction Industries and Resource Industries are solving customers’ toughest challenges through commercial excellence and advanced technology, driven by a highly skilled, dedicated global team. Learn more at www.caterpillar.com.
Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.
Press Inquiries:
Amy Doughty
Caterpillar Trade Press Media Representative
Amy.Doughty@cat.com
For Release: Africa, Middle East, Asia Pacific, South America, Southeast Asia, Eurasia
Release Number: 11PR26 - January 2026
The Latest Product News
-
New Cat® D11 Xe Electric Drive Dozer Delivers More Productivity and Lower Operating Costs
Cat® D11 XE electric drive dozer helps mining operations move more material with improved fuel efficiency and lower operating costs through an electric drivetrain designed for productivity and simplified service.
Learn More -
BHP, Rio Tinto and Caterpillar launch battery-electric haul truck trial in the Pilbara
BHP, Rio Tinto and Caterpillar have launched a trial of two Cat® 793 XE Early Learner battery-electric haul trucks at a mine-site demonstration in Western Australia’s Pilbara as part of an industry-first collaboration.
Learn More -
Caterpillar announces new Cat® M320 Wheel Excavator
The new Cat® M320 wheel excavator delivers enhanced ease of use, efficiency, stability and reduced operating costs.
Learn More -
Carmeuse Selects Caterpillar’s Autonomous Hauling Solution to Deploy at Drummond Island Operation
Caterpillar Inc. today announced an agreement with Carmeuse, a global leader in lime and limestone production, to deploy Caterpillar’s autonomous hauling solution at the Carmeuse Drummond Island quarry in Drummond, Michigan.
Learn More