Cat engines with ACERT Technology meet today's most stringent emissions reduction standards. And they're poised to take on tomorrow's challenges as well Caterpillar Brings Engines with ACERT Technology to Off-Road Machines

Cat® machines are rolling off assembly lines with the latest in engine technology. The first model to ship was the D8T.  Several other models followed suit including the D9T, 365, 385, and four Articulated Trucks.  As of the end of April, a total of 26 machine models are available!  Each of these machines use Caterpillar engines with ACERT™ Technology, the result of more than $500 million in research and development and more than 250 patents. The engines are compliant with the United States EPA Tier 3 emissions regulations governing off-road machines, which took effect January 1, 2005 for engines of 300 to 750 horsepower.

ACERT Technology is another example of why Caterpillar continues to be the North American leader in on-highway engines. Truck engines with ACERT Technology log more than 70 million miles each day. In fact, Caterpillar factories ship more than 16,000 of those engines each month. That on-highway record, coupled with Caterpillar's decades of experience in the off-road business, means customers will continue to receive the ultimate in engine performance and machine production.

Emissions regulations for machine engines are not new. The first went into effect in 1996, and Tier 2 regulations were applied in 2001. Those standards were met by adapting existing technologies, but the aggressive Tier 3 requirements dictated breakthroughs.

Caterpillar introduced ACERT Technology to meet EPA '04 regulations for on-highway trucks. Earlier, Caterpillar machine engines with ACERT Technology began field-testing across the United States, Canada and Europe. Now there are more than 350 such machines in the field. Combined, they have worked over 520,000 hours.  These machines are working in the multitude of applications typical for Cat equipment—from construction to mines to landfills. And they are working in a wide variety of conditions. One track-type tractor has performed successfully in a road-building project at 8,100 feet altitude.

ACERT Technology represents a series of evolutionary and incremental improvements developed by Caterpillar. For example:

  • The fuel system allows for multiple injections each combustion cycle. Small amounts of fuel are injected at precise times to achieve the combined goals of fuel economy and lower emissions.
     
  • An advanced air system provides more cool air in the combustion chamber. A wastegate turbocharger provides excellent low-end response.  In addition, crossflow cylinder heads provide a direct path of air to the engine. 

Caterpillar engineers worked with approximately 125 variables to find the optimum balance. There are more than 10 million possible combustion combinations. Those engineers were challenged by the highly intertwined relationship of (1) reduced emissions, (2) engine performance, (3) fuel efficiency and (4) engine durability. Those are not necessarily complimentary objectives. Improving emissions, for example, can have an adverse effect on fuel efficiency. Their overriding goal is no different than the goal Caterpillar has had since its inception—to provide customers with the lowest owning and operating costs, and the lowest cost per unit of material moved.

   Brochures
  
Title File Size File Type
» •  Proven to Perform - ACERT Technology for Off-Road Applications 518 KB PDF
» •  Cat® Industrial Engines with ACERT Technology 2 MB PDF
» •  Cat® Industrial Engine Ratings Guide (LECH3874-09) 941 KB PDF