Sabey Corporation developed Intergate.Manhattan into what is now the tallest data center in the world. Located in New York City, the facility presents a unique set of challenges including security, preservation and power loss. Sabey relies on its partnership with the local Cat® dealer, H.O. Penn, for emergency backup system support and critical data management.
There has been an increasing move toward natural gas fueled standby power systems in recent years. Typically installed with an automatic transfer switch (ATS) or paralleling switchgear control for multiple generators, these generator sets sense when a utility outage occurs and automatically starts the backup power generator system transferring power to the emergency source. When the normal grid power returns, the control system automatically switches back and shuts down the emergency generator.
Cat® Generator Sets Keep Caves Lit Up for Tourists
Natural Bridge Caverns added a new D200 GC diesel generator set to its fleet of five Cat generator sets to guarantee backup power. In the event of a power outage or interruption, the generator sets will ensure lighting, ticketing, and point-of-sale systems continue operation at under- and above-ground attractions.
Learn MoreCat® Dealer Delivers Rental Generators for Outdoor Music Concerts
The Shoshone-Bannock Casino Hotel not only turns to Cat® dealer Western States for permanent Cat® 3516 and C175 diesel generators to provide standby power, but also rents Cat XQ125 mobile generators to supply power for a stage, beer tents, and lighting equipment during large music concerts at its outdoor event venue.
Learn MoreCat® Mobile Generators Provide Power and Save Grain Following Deadly Tornado
A Cat® dealer helped Memphis-based Callan Salvage & Appraisal dispatch mobile generators to power Mayfield Grain. The portable power helped to save 6,800 trailer loads of grain worth more than $30 million.
Learn MoreAirport Upgrades Cat Power System For Maximum Reliability
The Kansas City International Airport relies on Cat generator sets and switchgear to deliver emergency backup power to the airfield. During a massive construction project that began in 2019, technicians from Cat® dealer Foley Power Solutions updated the electrical switchgear and genset control panels to ensure the system performs flawlessly.
Learn MoreProducing reliable power from 1600 to 2000 kVA at 50 Hz, our 3516 diesel generator sets are made to meet your mission critical, continuous, standby and prime applications. We've designed each to ISO 8528-5 transient response requirements and to accept 100% rated load in one step. Generator sets offer a low fuel consumption system.
Learn MoreUsing natural gas for combined heat and power (CHP) systems and emergency power for facilities, to renewable biogas energy to support the local grid, or electricity generated from coal mine gases, Caterpillar has a wide range of reliable gas power solutions.
Learn MoreFrom low energy gas-fueled combined heat and power (CHP) systems and emergency power for facilities, to renewable biogas energy to support the local grid, or electricity generated from coal mine gases, Caterpillar has a wide range of reliable gas power solutions.
Learn More