Caterpillar’s 140 Lever Motor Grader moves to the next generation
The new model, which features the hallmarks of efficiency, productivity and operator comfort, will launch in early 2026.
Highlights
- Increased uptime includes extended and synchronized maintenance intervals plus centralized success service points
- Integrated optional rear-, front-, and 360-degree-vision cameras, enhanced visibility and redesigned HVAC system and seat adjustment options in the cab
- Powertrain choice of tandem or All-Wheel Drive to accommodate jobsite applications
IRVING, Texas, August 20, 2025―Caterpillar is announcing its new Cat® 140 LVR Motor Grader, upgrading it to the next generation platform. The new model, which features the hallmarks of efficiency, productivity and operator comfort, will launch in early 2026.
Pablo dos Santos
Global Product Application Specialist
Caterpillar
“Over the years, customers have shown that the 140’s usefulness and flexibility have few limits. Its frame lends itself to easy transportation, and its power and performance have seen it put to work in everything from snow clearance to grading operations, in addition to its everyday use in roadbuilding and ditching.
Dos Santos says the machine’s versatility, which has made it very popular with rental fleets, as well as government and municipal contracts, will be enhanced by moving to the next generation platform.
Safety and efficiency rely on good visibility, so the Cat 140 Motor Grader features the successful cab design from the 120 next gen models. Larger windows provide better visibility out of the cab, ensuring better all-round views, including moldboard and tires, while an as-standard rearview camera augments direct lines of sight.
The camera feed is integrated into the 10-inch touchscreen, which also provides operator access to other next generation functions such as Cat Grade. A new seat takes advantage of the next gen cab’s foot space and hip room, offering a variety of adjustments to improve operator comfort and help reduce fatigue. The cab features revised seatbelt and safety harness options.
The new Cat 140 continues its proven design and reliability to help with low operating costs, coupled with favorable fuel efficiency. The 140 features banked and centralized access checkpoints that can help make daily maintenance a breeze rather than a bind.
What’s more, the new 140 provides a ‘sweet spot’ power-to-weight ratio with excellent fuel consumption rates, notes dos Santos. “There is a lot of good information collected so far from the multiple machines being tested around the world, with more than 40,000 hours accumulated so far.”
The new Cat 140 also offers expanded technology capabilities, from simple features to improve operator’s comfort, like the stable blade, to fully calibrated 3D systems to help reduce the total cost of ownership.
Pablo dos Santos
Global Product Application Specialist
Caterpillar
A Century of Innovations
Caterpillar began manufacturing motor graders in 1931 with the No. 9 Cat Auto Patrol. The first motor graders boasted lever and steering wheel controls and a 9-foot moldboard. Presently, Caterpillar manufactures 13 motor grader models in facilities across the globe.
For more information about the Cat 140 LVR Motor Grader, contact a Cat dealer or visit: www.cat.com
# # #
About Caterpillar:
With 2024 sales and revenues of $64.8 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels at caterpillar.com/en/news/social-media.html.
Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.
Press Inquiries:
Kate Kenny
Caterpillar Trade Press Media Representative
Kenny_Kate@cat.com
Release Number: 189PR25 — August 2025
For Release: Worldwide excluding Europe
The Latest Product News
-
Caterpillar updates Cat® AP1000 and AP1055 pavers, introduces new smooth SDX plates and collision mitigation
Caterpillar announces multiple design enhancements for the Cat® AP1000 wheel and AP1055 track asphalt pavers, targeting increases in reliability and longevity as well as simplified maintenance.
Learn More -
Caterpillar to preview three new compact machine models at CONEXPO-CON/AGG
Helping customers reshape what’s possible, Caterpillar previews three new compact equipment models in its West Hall CONEXPO-CON/AGG display, booth W40416.
Learn More -
Caterpillar expands Next Generation dozer Electric Drive lineup with introduction of the Cat® D8 XE
Caterpillar has announced the latest addition to its Next Generation dozer range, the Cat® D8 XE, reinforcing its commitment to the fuel-saving and maintenance-easing benefits of Electric Drive powertrain technology.
Learn More -
Caterpillar launches six new Cat® attachments for next generation Cat machines
Caterpillar announces a range of new Cat® attachments to increase application flexibility of its next generation skid steer loader (SSL) and compact track loader (CTL), mini hydraulic excavators and certain backhoe loader models.
Learn More