Building the Future: Our Most Impactful Projects
Not many companies can say they’ve helped build a better world. But for a hundred years, that’s precisely what Caterpillar has been doing. Here are just some of those historic contributions.
Modern Marvels: Caterpillar’s Work on Large-Scale Dam Construction
Caterpillar has been involved in building three of the most famous dams in the world.
THE HOOVER DAM
The Hoover Dam was built in the 1930s and was, for some time, the tallest dam in the world at 726 feet (221m) tall and 1,244 feet (400m) long.
THE THREE GORGES DAM
Even larger, at 594 feet (181 m) high and over 1.4 miles (2.3 km) long, is the Three Gorges Dam in China, which used more than 300 Cat® machines during its 12-year-long construction.
THE ITAIPU DAM
And even bigger still, is Itaipu Dam. Situated between Brazil and Paraguay, Itaipu Dam is one of the world’s largest hydroelectric projects. While only 643 feet (196m) tall, it’s an astonishing 4.9 miles (7.9 km) long. And, of course, Cat machines were used to help build it. Completed in 1982, today it’s still regarded as one of the Modern Wonders of the World.
Operation Deep Freeze: Bold Innovations in Antarctica
Let’s travel back to the 1950s: a time of geopolitical tensions and remarkable collaboration among 40 nations. This was the era of Operation Deep Freeze, a groundbreaking initiative that sought to establish American research stations in Antarctica. Caterpillar’s role was to build custom track-type tractors and diesel-electric sets that would work 24 hours a day, seven days a week, at temperatures of -65o F (-53oC) and below.
The resulting low-ground-pressure (LGP) tractors were built with wide tracks that distributed the machine’s weight over a larger surface of the ice and snow to avoid damaging the terrain or sinking. This technology helped construct roads and bases, haul supplies, maintain airstrips and doze snow, amongst other things. The electric sets powered everything from heating and lights to communication systems and radar.
Cat® machines still support Antarctic research stations today.
Taking Cat® Technology to the Moon & Back
Rather apt for a company known as earthmoving experts, it’s been said that Caterpillar moved heaven and earth in 1969 to help Apollo 11 astronauts get to the moon and back.
Cat diesel-electric sets helped power communications between NASA's worldwide network tracking stations and the Apollo 11 spacecraft, relaying commands from the flight director and the spacecraft during the whole journey.
Years later, Caterpillar’s space technology contributions and collaboration with NASA have continued. In 2007, our autonomy and robotics experts helped NASA develop lunar excavation and construction capabilities. In 2024, NASA launched a lunar lander with the Cat logo emblazoned on the side in honor of a long-standing relationship.
The Road Ahead: Infinite Possibilities
And now, in our centennial year, as we look to the future, the really exciting question isn’t, what lies ahead, but how can we continue to collaborate and innovate for a brighter tomorrow. As we stay true our steadfast commitment, to help build a sustainable and prosperous future for all.
Related Stories
-
The Legacy of Holt & Best
Benjamin Holt and C.L. Best changed the industry over 100 years ago – first as competitors, and then as the founders of Caterpillar. Their passion for customers and innovation lives on today.
READ MORE -
Mongolia Man-Made Lake
Mongolia's largest man-made lake was created using a Cat® D8R Dozer as an act of environmental rehabilitation. The man-made lake was once a functional mine - see how it was done!
READ ON -
Building a New Dam in the Alps
Everything about the Kühtai Dam Project is huge. From its estimated €1bn cost, to its location, 2,200 meters up in the Austrian Alps, to the number and size of Cat® machines they’re using.
Learn More