For Release: August 20, 2025
IRVING, TEXAS—Caterpillar Inc. today announced the introduction of the new Cat® D1500 diesel generator set, which offers best-in-class power density by delivering 1.5 MW of standby power from a compact 32.1-liter Cat C32B engine. It occupies up to 13% less floor space and is up to 32% lighter than the previous model at this power rating, making it ideal for locations where space is constrained.
The reduced weight provides economic benefits for customers, including lower shipping and installation costs, and it can also reduce setup and structural support requirements. Now available at Cat dealers in North America, the Cat D1500 is designed for a wide range of 60 Hz applications.
The Cat D1500 generator set offers numerous features, making it ideal for supplying standby power. It conforms to ISO 8528-5 steady state and transient response requirements, thereby ensuring that operational continuity is maintained during power outages or peak load times.
The generator set complies with NFPA 110 Level 1 Type 10 standards for fast power restoration during outages. It is ULC 2200 Listed for both the US and Canada, providing enhanced safety assurance. It also meets the U.S. EPA Tier 2 emission standard for stationary emergency use.
“In this evolving energy landscape where space is at a premium, the Cat D1500’s compact size and high power density make it an ideal choice for customers looking to add reliable standby power,” said Melissa Busen, senior vice president for Caterpillar’s Electric Power Division.
Customers will be able to remotely monitor, locate, and manage the Cat D1500 generator set through an easy-to-use web interface or mobile app. Available with a subscription, it enables users to track performance and troubleshoot remotely, ultimately avoiding the costly implications of downtime.
The generator set is equipped with a standard controller that automatically starts the unit during a power outage to deliver reliable backup power. For greater control and efficiency, it can be configured with Cat Energy Control System (ECS), offering enhanced monitoring, remote access, and load management capabilities. Cat ECS controllers also support paralleling and seamless integration with power management systems, making them ideal for more complex standby power applications.
For more information, visit https://www.cat.com/en_AU/products/new/power-systems/electric-power/diesel-generator-sets.html.
###
With 2024 sales and revenues of $64.8 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For nearly 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels.
© 2025 Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
Press Inquiries
Bob Chase
Gelia
bchase@gelia.com
Pooja Das Sharma
Caterpillar Inc.
Pooja.DasSharma@cat.com