Made from through-hardened DH-2 steel, these new ground engaging tools (GET) from Caterpillar are thicker and provide similar or better life to the standard cutting edge option.
IRVING, Texas, May 13, 2025―The new Cat® Single Life Cutting Edges for Cat medium wheel loaders feature a single bevel design that eliminates the need to monitor wear for flipping edges. Made from through-hardened DH-2 steel, these new ground engaging tools (GET) from Caterpillar are thicker and provide similar or better life to the standard cutting edge option. The new Single Life Cutting Edges endure a wide range of applications, including both high impact and abrasion, for the Cat 950, 962, 966, 972, 980 and 982 loader series, including XE and GC models.
Tilak Inturi
Senior Parts and Service Marketing Manager
Caterpillar
New Cat Single Life Cutting Edges offer similar or better wear life, but at a lower price point, than standard cutting edge systems. Reducing the need to monitor wear, the single bevel simplifies maintenance, since there is no downtime or need for new hardware to flip the edges mid-life. The two cutting edge pieces fit the bucket with no end bits required, and the new system is backed by a Cat limited warranty.
The new single life edges expand Caterpillar’s broad portfolio of edge solutions, designed to increase the wheel loader’s productivity by reducing operating and maintenance interval costs. The adaptable new design is retrofittable to aftermarket buckets with the same hole pattern.
More information on the new Cat Single Life Cutting Edges can be found by contacting a Cat dealer or visiting cat.com.
# # #
About Caterpillar:
With 2024 sales and revenues of $64.8 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels at caterpillar.com/en/news/social-media.html.
NOTE TO EDITORS: Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.
The best machine operators across North America gathered in Clayton, NC to forge their legacy and prove their mastery of both equipment and technology.
Learn MoreCaterpillar introduces a smarter articulated truck design with built-in automatic features for the next generation Cat® 725, 730, 730 EJ and 735 models.
Learn MoreCaterpillar is announcing its new Cat® 140 LVR Motor Grader, upgrading it to the next generation platform.
Learn MoreThe new heavy-duty Cat® 980 GC Wheel Loader offers low fuel consumption with an on-demand fan, load-sensing hydraulics, intuitive controls and Performance Series buckets.
Learn More