The new model, which features the next generation hallmarks of efficiency, productivity and operator comfort, will debut at bauma 2025 in Munich.
IRVING, Texas, March 7, 2025―Caterpillar will be launching its new Cat® 140 Motor Grader, upgrading it to the next generation platform. The new model, which features the next generation hallmarks of efficiency, productivity and operator comfort, will debut at bauma 2025 in Munich.
Pablo dos Santos
Global Product Application Specialist
Caterpillar
Over the years, customers have shown that the 140’s usefulness and flexibility has few limits. Its frame lends itself to easy transportation, and its power and performance have seen it put to work in everything from snow clearance to sugarcane operations, in addition to its everyday use in roadbuilding and ditching.
Pablo dos Santos
Global Product Application Specialist
Caterpillar
Safety and efficiency rely on good visibility, so the Cat 140 Motor Grader features the highly successful cab design from the 120 next gen models. Larger windows provide better visibility out of the cab, ensuring better all-round views, including mouldboard and tyres, while an as-standard rearview camera augments direct lines of sight.
The camera feed is integrated into the 10-inch touchscreen, which also provides operator access to other next generation functions such as Cat Grade. A new seat takes advantage of the next gen cab’s greater footspace and hip room, offering a variety of adjustments to improve operator comfort and reduce fatigue. The cab features revised seatbelt and safety harness options.
Also benefiting from the next gen upgrade are the 140’s joystick controls. While Caterpillar has stuck with its industry-exclusive three axis joystick system, which studies show is more ergonomical for operators than levers and a steering wheel, the 140 makes several updates to the joysticks themselves to help further boost productivity.
The new Cat 140 continues its proven design and exceptional reliability to ensure low operating costs coupled with favourable fuel efficiency. The 140 features banked and centralised access checkpoints that make daily maintenance a breeze rather than a bind.
Pablo dos Santos
Global Product Application Specialist
Caterpillar
There is a lot of good information collected so far from the multiple machines being tested in the world with more than 40.000 hours accumulated so far.
The new Cat 140 also offers expanded technology capabilities, from simple features to improve operator’s comfort, like the stable blade, to fully calibrated 3D systems for reduced total cost of ownership.
Pablo dos Santos
Global Product Application Specialist
Caterpillar
The new Cat 140 is due for production in Q1, 2026.
Caterpillar began manufacturing motor graders in 1931 with the No. 9 Cat Auto Patrol. The first motor graders boasted lever and steering wheel controls and a 9-foot mouldboard. Presently, Caterpillar manufactures 13 motor grader models in facilities across the globe.
For more information about the Cat 140 Motor Grader, contact a Cat dealer or visit: www.cat.com
# # #
About Caterpillar:
With 2024 sales and revenues of $64.8 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels at caterpillar.com/en/news/social-media.html.
NOTE TO EDITORS: Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.
Held on Caterpillar grounds at the Malaga Demonstration and Learning Centre, the Global Operator Challenge (GOC) saw the 20 best operators from Europe, Africa and Middle East compete in the semifinal competitions.
Learn MoreBuilt to deliver a long reach required for barge loading/unloading and large scrapyard applications, the new Cat® MH3295 Material Handler will feature a dedicated swing pump for smooth, coordinated movement and a wide track undercarriage for optimum stability and performance.
Learn MoreCaterpillar introduces a smarter articulated truck design with built-in automatic features for the next generation Cat® 725, 730, 730 EJ and 735 models.
Learn MoreThe new heavy-duty Cat® 980 GC Wheel Loader offers low fuel consumption with an on-demand fan, load-sensing hydraulics, intuitive controls and Performance Series buckets.
Learn More