Held on Caterpillar grounds at the Malaga Demonstration and Learning Centre, the Global Operator Challenge (GOC) saw the 20 best operators from Europe, Africa and Middle East compete in the semifinal competitions.
IRVING, Texas, October 9, 2025―The best machine operators from across Europe, Africa and Middle East gathered in Malaga, Spain to forge their legacy and prove their mastery of both equipment and technology. The 20 competitors first had to win local Cat® dealer competitions to qualify for regionals. Only three emerged victorious and earned the right to advance to the final round in the Caterpillar Global Operator Challenge (GOC) to be held in Las Vegas in March 2026. The GOC finals will take place during CONEXPO-CON/AGG inside Caterpillar’s 70,000 ft2 outdoor exhibit, F29029, in the Festival Lot.
The overall champion of the Malaga based competition was Gunter Dewit from Belgium representing dealer Bergerat Monnoyeur Belgium. Dewit finished the four GOC events with the lowest points total of 983, which is a combination of time and penalties.
At the same time, both Nicolai Thomsen from Denmark, representing dealer Zeppelin Denmark, completed the challenges with 1048 points, emerging as the first runner up and Sebastian Behr from Germany, representing dealer Zeppelin GmbH with 1101 points emerged as the second runner up. Both of these operators will also progress to the finals.
All competitors completed the same four Challenge events using Cat® equipment and technology.
Serena Janssen
Industry Solutions lead
Caterpillar
The Touchdown Challenge saw competitors using a Cat 320 hydraulic excavator fitted with 3D GPS to pick up two rugby balls consecutively and drop them in a nearby basket. Contestants then needs to touch two targets using the machines 3D GPS technology.
In celebration of a century of earthmoving excellence, the Centennial Push Challenge had operators put a Cat D4 dozer through a pre-determined course within a specified time-frame. Operators were able to use optional aids via Steer Assist and Slope Assist, which are built into the machine to help with precision maneuvers.
Featuring a Cat 938 small wheel loader, the Loader Labyrinth Challenge highlighted the agility and adaptability of the operators as they navigated a dual-phase course. Starting with a bucket, participants loaded and hauled material along a marked path before dumping it into a Cat off-highway truck. The challenge then shifted to precision handling, where operators had to swap their bucket for forks and transport a pipe across a designated route and place it accurately on the ground. After reversing the process and reconnecting the bucket safely, operators reversed through the course to the original starting position. It was a test of speed, control, and seamless equipment transitions.
The Articulator Challenge featured the recently announced next generation 730 articulated truck where competitors maneuvered the machine through a designated course. Operators had to avoid obstacles along the way before safely and precisely reversing to a pre-determined dumping area where they had to safely lower the truck body completely before returning to the travel position and coming parking correctly under a wheeled loader at the end position.
Regional competitions across the globe determine the nine operators who will compete in the global finals. The winner receives either a $10,000 cash prize or an equal value trip for two where Caterpillar has a location worldwide.
For more information about the Global Operator Challenge visit www.cat.com/operatorchallenge.
# # #
About Caterpillar:
With 2024 sales and revenues of $64.8 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels at caterpillar.com/en/news/social-media.html.
Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.
It’s all about getting back to work quicker with the new Cat® Track Clamp Master Link assembly, designed to improve track installation efficiency in the field by eliminating the need for a portable field press.
Learn MoreDelivering powerful performance, the Cat® 325 Excavator features easy-to-use standard technology like Cat Grade with 2D, Grade Assist, Lift Assist and Payload to help boost productivity by allowing operators to work accurately, efficiently and quickly.
Learn MoreBuilt to deliver a long reach required for barge loading/unloading and large scrapyard applications, the new Cat® MH3295 Material Handler will feature a dedicated swing pump for smooth, coordinated movement and a wide track undercarriage for optimum stability and performance.
Learn MoreCaterpillar introduces a smarter articulated truck design with built-in automatic features for the next generation Cat® 725, 730, 730 EJ and 735 models.
Learn More