Long heavy-duty undercarriage with oversized 203-mm (8-in) track pitch delivers outstanding stability and durability in harsh, uneven ground conditions, including site preparation, land clearing and forestry.
IRVING, Texas, November 10, 2025―Delivering powerful performance, the Cat® 325 Excavator features easy-to-use standard technology like Cat Grade with 2D, Grade Assist, Lift Assist and Payload to help boost productivity by allowing operators to work accurately, efficiently and quickly. Long heavy-duty undercarriage with oversized 203-mm (8-in) track pitch delivers outstanding stability and durability in harsh, uneven ground conditions, including site preparation, land clearing and forestry. Equipping the 325 with the optional blade simplifies backfilling and helps keep the machine leveled when working on slopes.
Featuring a 7.5-tonne (16,540-lb) counterweight, the new configuration enhances balance and control even when equipped with attachments like a blade, Variable Angle Boom (VAB), heavy-duty stick, bucket thumbs, or quick coupler. The new configuration can be fitted with either Reach or VAB fronts, with or without a blade, and comes with a thumb-ready stick and quick coupler circuit preinstalled from the factory, reducing the need for aftermarket modifications. Stability equivalent to the 325 with an 8.3-tonne (18,300-lb) counterweight and standard undercarriage, its larger final drives increase drawbar pull to better climb grades, and higher swing torque maintains swing uphill capabilities.
Adrian Grigorita
Vice President
Product Management for Medium Hydraulic Excavators Caterpillar
When equipped with the latest HD configuration, the compact radius Cat 325 Excavator delivers heavy-duty performance with unmatched versatility when working in tight spaces. It offers all the benefits expected by operators – factory-integrated technology to boost productivity, extended maintenance intervals to help keep operating costs low, and electrohydraulic efficiency for smooth, precise operation.
The excavator’s electro-hydraulic pump and main control valve work together to optimize power and efficiency for the 325, delivering the performance needed. By automatically adjusting engine power to match hydraulic demands, Smart Mode operation helps lower fuel consumption.
Longer fuel life, hydraulic oil and air filters for the 325 reduce the number of filters over the life of the machine to deliver low maintenance costs. No pilot or case drain filters result in fewer filters to replace over the machine’s service life, and ground-level engine oil level checks keep the operator safely on the ground when performing daily maintenance inspections.
More information on the Cat 325 Excavator can be found by contacting a Cat dealer or visiting cat.com.
# # #
About Caterpillar:
With 2024 sales and revenues of $64.8 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels at caterpillar.com/en/news/social-media.html.
Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.
It’s all about getting back to work quicker with the new Cat® Track Clamp Master Link assembly, designed to improve track installation efficiency in the field by eliminating the need for a portable field press.
Learn MoreHeld on Caterpillar grounds at the Malaga Demonstration and Learning Centre, the Global Operator Challenge (GOC) saw the 20 best operators from Europe, Africa and Middle East compete in the semifinal competitions.
Learn MoreBuilt to deliver a long reach required for barge loading/unloading and large scrapyard applications, the new Cat® MH3295 Material Handler will feature a dedicated swing pump for smooth, coordinated movement and a wide track undercarriage for optimum stability and performance.
Learn MoreCaterpillar introduces a smarter articulated truck design with built-in automatic features for the next generation Cat® 725, 730, 730 EJ and 735 models.
Learn More