If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
For Worldwide Release: September 2019
Houston, Texas – Caterpillar Oil & Gas is pleased to announce the next generation of human-machine interface (HMI) panels available as an integrated component on select gas compression models. The easy to use touchscreen display performs the functions of the customer version of Cat® Electronic Technician. Now, with the HMI panel integration, controlling the engine and monitoring the system’s status is at the users’ fingertips. The new HMI panel is now available on the CG137-8 and will be released as an offering for additional gas compression models at a later date.
Available as a standard offering, the 8” color touchscreen HMI panel was intuitively designed with easy to understand icons and labeling. ECM configurations, PMS settings, and service tests are also accessible through the display allowing for an easy way for users to monitor engines.
By integrating the HMI panel on the gas compression product line, functionality will be identical. The commonality will allow for similar user experience on the products. When designing the HMI panel, user experience was key. “Our goal was to enhance the user experience by providing an intuitive interface that would look and function the same across our gas compression product line,” said Michael Coppinger, Caterpillar Product Definition Manager. “Whether you have a mixed fleet of Caterpillar engines, or you’re responsible for one site with various G3600 models, with a common NextGen HMI you can walk up to a unit and instantly be familiar with the engine interface display,” said Michael.
Additional features include the ability to remotely reset the engine, log data, and view histograms and snapshot data. Users can also perform alarm and shutdown resets without having to power cycle the engine when ready to be used. To conserve batteries, users can select the sleep mode power option. “By integrating a number of features, which traditionally required the use of a laptop and Cat Electronic Technician, operators and service technicians will benefit from the ease of making configuration changes, accessing histograms, or viewing status reports, all via the 8-inch touchscreen display,” said Michael.
Optional attachments are also available for the panel including a front and backplate with control switches and a fully enclosed metal box for the panel.
Reduce maintenance time and costs with the next generation of HMI panels and make your job easier. Retrofit options are in development and upgrades from the 7” HMI display to the 8” panel can be completed as an easy replacement. To learn more about the HMI panel for gas compression, talk to one of our product experts at booth #413 at the 2019 Gas Machinery Research Council (GMRC) Convention in San Antonio, Texas during the week September 29th – October 2nd.
About Caterpillar Oil & Gas
Caterpillar Oil & Gas, Caterpillar Inc.’s oil and gas division with headquarters in Houston, Texas, consolidates all the sales and service activities for Cat oil and gas power solutions. Since the 1930s, Caterpillar has manufactured engines for the oilfield and today provides premier power solutions with outputs from 31 to 16,000 kW. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in the drilling, production, well service and gas compression segments. More information is available at: cat.com
About Caterpillar
For more than 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2018 sales and revenues of $54.722 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three primary segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
Caterpillar. All Rights Reserved. CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Yellow”, the “Power Edge” and Cat “Modern Hex” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2019 Caterpillar
All Rights Reserved
Press Inquiries |
Danielle Wills |