If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Dozer tracks are like a chainsaw. If the blade is too loose, you’re going to throw it and suffer downtime getting it back on. Too tight, and you’re putting extra wear on both the tracks and the power train. Here’s how to check dozer track tension.
Estimated read time: 3 minutes
Bulldozer tracks are amazing to see in action. They allow your machine to work hard in difficult terrain and conditions.
And dozer tracks need care and attention to keep working as hard as you need them to. Remember that they’re constantly in contact with whatever you’re pushing, grading or spreading. If the tracks are too loose or too tight, you risk throwing the track while putting premature wear on the carrier rollers, frame and power train. It’s also a safety issue.
On top of all this, a badly adjusted track is just bad for your business. You could be looking at unplanned maintenance and repair costs. Luckily, there's a simple way to check your Cat® dozer’s track tension. No need to haul your equipment off to the shop.
First off, daily maintenance increases the life of seals and components. Here are some tips:
Clean the undercarriage every day.
Use a shovel to remove excess dirt and debris from the track roller frame and equalizer bar ends, pivot shaft, track idlers and rollers.
If the tracks are caked with heavy mud, spray them out with water, but take care not to spray seals or the track pin, roller or idler stoppers.
It’s also important to inspect the track. Some best practices are:
Listen for excessive squealing during operation. That’s usually an indication of dry joints that need attention.
After you shut the machine down, lightly feel the ends of the pins and bushings to see if they’re excessively hot.
Check the track roller frame for any cracks or leaks.
Make sure the equalizer bar pin is in good condition.
Put a string or a straight edge on the grousers to check for consistent wear patterns. See photo above for areas to measure on a track with a carrier roller.
If your bulldozer doesn’t have a carrier roller, measure the sag between the sprocket and the front idler.
Keep in mind that there are different dimensions for machines with and without carrier rollers.
Check your Operation and Maintenance Manual (OMM) for more details about measuring tension.
Also check your OMM for proper dimensions for your undercarriage type.
If you check your OMM and determine the track tension isn’t right, here’s how to proceed.
If the track is too tight:
Remove the access cover to the track adjustment valve.
Add multipurpose grease to the valve until you reach the correct dimensions.
Operate the machine back and forth to equalize the pressure of the grease in the track adjustment valve. Do not allow the machine to coast or use the brakes.
Remeasure the track dimensions to confirm they are now correct.
It the track is too loose:
Remove the access cover to the track adjustment valve.
Loosen the relief valve slowly and allow grease to escape. This will allow the front track roller frame to retract.
Close the relief valve once you have reached the proper track tension.
Learn more about the Cat services that are available for your dozer.
Get the most from your bulldozer with operating tips, safety advice, maintenance help and much more.
How To Adjust Controls To Fit Operator Preference on Cat® 926, 930, 938 Small Wheel Loaders
Learn MoreHow To Utilize Auto Engine Mode on Cat® 926, 930, 938 Small Wheel Loaders
Learn MoreHow To Leverage Multi View 360 Degree Cameras on Cat® 926, 930, 938 Small Wheel Loaders
Learn MoreHow To Utilize Operator Not Present Mode on Cat® 926, 930, 938 Small Wheel Loaders
Learn MoreGain unlimited access to must-know information about your machine. Find ideas you can put to work on the job right away, including business insights.