Caterpillar announces updates to Cat® 5- to 10-tonne class mini hydraulic excavators
The compact radius Cat 305 CR now joins the 6- to 10-tonne class models to offer mini hydraulic excavator (MHE) ease-of-use (EOU) E-Fence and Indicate features for software-enabled attachment versions.
Highlights
- 5-tonne compact radius Cat 305 CR now offers ease-of-use (EOU) features
- Cat 308 CR can be equipped with an angle blade
- New camera, engine and third auxiliary features for 8- to 10-tonne models
IRVING, Texas, October 7, 2025― Caterpillar is announcing multiple enhancements to its Cat® 305 CR, 308 CR, 309 CR and 310 Mini Hydraulic Excavator models. The compact radius Cat 305 CR now joins the 6- to 10-tonne class models to offer mini hydraulic excavator (MHE) ease-of-use (EOU) E-Fence and Indicate features for software-enabled attachment versions. The 305 CR now ships from the factory EOU ready for cab and premium canopy designs or can be ordered from the factory already installed.
Automatically constraining machine motion within preset boundaries, E-Fence is designed to allow operators the ability to work confidently and efficiently by avoiding structures overhead, underground, in front, or to the left or right of the excavator. E-Fence features include:
- Ceiling – helps operators avoid overhead obstacles such as powerlines, ceilings or tree limbs.
- Floor – defined depth limits help protect underground fiberoptic cables and utilities.
- Wall – operating limits protects structures in front of the excavator.
- Swing – ideal for avoiding swinging into live traffic areas or walkways and to help with truck loading.
An entry-level grade system now available for the 305 CR, Indicate, gives operators visual and audible indications to bucket position, relative to target grade, to assist with meeting exact specifications the first time. The operator selects target depth and slope from the in-cab guidance system, and the monitor provides real-time feedback.
Taking the EOU Indicate to the next level, a Laser Catcher option is available for all next generation Cat EOU models in the 5- to 10-tonne class. Working with a laser transmitter, Laser Catcher may provide customers with greater peace of mind when working on large jobsites that require multiple excavator repositions. It can be ordered from the factory or installed via an aftermarket kit and retrofitted to first-production EOU machines.
8- to 10-tonne class enhancements
Today’s compact radius Cat 308 CR and 309 CR plus the 310 mini hydraulic excavators are now powered by the new Cat C2.8 engine, offering the same ratings and performance as the previous Cat C3.3B power unit. Meeting U.S. EPA Tier 4 Final and Stage V emissions standards, the C2.8 features a “fit for life” diesel oxidation catalyst (DOC) and diesel particulate filter (DPF) that requires no maintenance, reducing service requirements and costs.
A third auxiliary hydraulic option is available to support customers using complex hydromechanical attachments. These next gen excavators also feature a standard rearview camera to help improve operator visibility and safety while reversing the excavator. Additionally, the 310 now includes a side-view camera as standard, while the side-view camera can be optionally added to 308 CR and 309 CR machines.
The next generation 308 CR will offer an angle blade option to help with backfilling material. With Stick Steer and blade control in the right joystick, operators can control the machine like a small dozer. The option comes with dozer float to help with grading and a three-piece bolt-on cutting edge that can be inverted and reversed to extend wear life.
Next level performance
These enhancements can elevate the performance of a next generation Cat mini hydraulic excavator line that introduced four industry-first features:
- Stick Steer – simplifying machine control, Cat Stick Steer System enables the operator to switch from conventional level/foot-pedal steering controls to low-effort joystick operation at the touch of a button.
- Cruise control – a standard feature minimizing operator interaction when traveling longer distances between work locations.
- Operator adjustable settings – a large touchscreen display provides intuitive machine function control and easy monitoring of critical operating parameters.
Limited edition “Centennial Grey” Cat 305 CR and 308 CR mini hydraulic excavator units will be on display at the Utility Exposition, October 7-9, and Equip Exposition, October 21-24, in Louisville, Ky. Attendees can operate the limited edition 308 CR model with angle blade inside the Cat demonstration exhibit area.
More information on the software updates for the Cat 305 CR, 308 CR, 309, CR and 310 mini hydraulic excavators can be found by contacting a Cat dealer or visiting cat.com.
# # #
About Caterpillar:
With 2024 sales and revenues of $64.8 billion, Caterpillar Inc. is the world’s leading manufacturer of construction and mining equipment, off-highway diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. For 100 years, we’ve been helping customers build a better, more sustainable world and are committed and contributing to a reduced-carbon future. Our innovative products and services, backed by our global dealer network, provide exceptional value that helps customers succeed. Caterpillar does business on every continent, principally operating through three primary segments – Construction Industries, Resource Industries and Energy & Transportation – and providing financing and related services through our Financial Products segment. Visit us at caterpillar.com or join the conversation on our social media channels at caterpillar.com/en/news/social-media.html.
Caterpillar rolls out products and services in each of its regions at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from its independent dealer network, plants, and marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with a Cat dealer for product availability and specifications.
CAT, CATERPILLAR, LET’S DO THE WORK, their respective logos, “Caterpillar Corporate Yellow,” the “Power Edge” and Cat “Modern Hex” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
VisionLink is a trademark of Caterpillar Inc., registered in the United States and in other countries.
Press Inquiries:
Johanna Kelly
Caterpillar Trade Press Media Representative
Kelly_Johanna_L@cat.com
For Release: North America
Release Number: 209PR25 — October 2025
The Latest Product News
-
New Cat® 301 Compact Radius Micro Excavator Offers Performance in Confined Spaces
The Cat 301 CR delivers advanced machine performance for indoor, demolition, agricultural and landscaping applications through simple, easy-to-use operating systems.
Learn More -
New Cat® 253 Compact Track Loader Expands LINE With Focus on Grading and Stability Performance
The new Cat® 253 compact track loader (CTL) offers a 2,006-lb (910-kg) rated operating capacity and an operating weight of 9,343 lb (4,238 kg), supporting easier transport between jobsites.
Learn More -
New Cat® 302.4 Compact Radius and 302.6 Mini Excavators Offer Enhanced Performance
The new Cat 302.4 Compact Radius (CR) and 302.6 mini excavators give customers two additional solutions in the 2.4- and 2.6-ton class sizes.
Learn More -
New Cat® Tul100 Compact Utility Loader Provides Solutions in Tight Space Applications
The new Cat® TUL100 compact utility loader is designed to deliver power and performance in tight spaces with reliability and durability.
Learn More