How to Install Rubber Tracks on a Compact Track Loader
Estimated read time: 2 minutes
Your Cat® compact track loader is built to get the job done, but over time, even the most durable rubber tracks wear down. When that happens, you can replace them yourself with the right tools and know-how.
In this video, we’ll show you how to remove and install rubber tracks on a Cat 299D3 Compact Track Loader. The same basic steps apply to most Cat Compact Track Loader models, so you can follow along no matter which one you run. You’ll see how to safely detension and remove old tracks, fit the new ones, and set the proper track tension for smooth, dependable operation. All so you can get back to work as soon and as safely as possible.
How to Remove Rubber Tracks
First, position your equipment on firm, level ground. For this service, remove any attachments from the quick coupler. Raise the loader arms and install the brace.
Shut off the engine and place direction control in neutral.
Use a suitable lifting device to raise the loader about 50 mm (2 inches) off the ground.
Detension the track by releasing grease from the adjustment valve.
Place the track bar tools, skipping two teeth between each.
Rotate the track toward the idler you want to use for removal.
Once the three bars are around the idler, make sure all surrounding teeth are disengaged.
Use a pry bar to continue disengaging the track. Use cribbing to support the weight.
Remove the rubber track and repeat the process on the other side.
How to Install Rubber Tracks
Position the track so the track lugs are inside the rear idler.
Position the front of the track onto the front idler so the teeth are against it.
Lift the track with a suitable lifting device to reengage the teeth.
Align the track with the grooves and place the tools above the idler, skipping two teeth between each.
Rotate the track toward the idler to allow the teeth to fall into place.
Use a pry bar to continue setting the track in position.
Once the track is properly installed, remove all tools.
Tighten the grease fitting and pump in grease until the track is properly tensioned.
Check track tension by measuring sag from the middle roller and add or remove grease as needed.
Explore everything you need to know about Cat rubber tracks.
Q: How do I replace rubber tracks on a Cat compact track loader?
A: Position the machine on level ground, remove attachments, brace the arms, detension the track, and use tools to disengage it from the idler. Then install the new track by aligning with the idlers, reengaging the teeth and tightening the grease fitting to adjust tension.
Q: What tools are needed for Cat rubber track installation?
A: You’ll need a suitable lifting device, track bar tools, a pry bar and cribbing to safely support the track during removal and installation.
Q: How do I check proper track tension after installing new rubber tracks?
A: Measure the sag from the middle roller. Adjust by adding or removing grease at the fitting until the track is correctly tensioned.
Q: How often should rubber tracks on a Cat loader be replaced?
A: Replacement timing depends on operating conditions and wear. Inspect your tracks regularly for cracks, missing lugs or loose fit and refer to your Operation and Maintenance Manual (OMM) for service intervals.
Q: Is it safe to replace Cat rubber tracks yourself?
A: Yes, if you follow the Operation and Maintenance Manual, wear personal protective equipment (PPE) and use the right tools. Always work on level ground and ensure the machine is braced and lifted securely.