For Release in North America: October 2017
Release Number: 562PR17
The Cat® 303E CR mini hydraulic excavator has been reduced in weight to accommodate customers who require a maximum 10,000-lb (4 536-kg) transport weight—yet performance of the lighter excavator has not been compromised when compared to the current model.
In most states a loaded trailer of more than 10,000 lb (4 536 kg) requires the tow vehicle driver to have a Commercial Drivers License (CDL). The new 303E CR weighs 6,750 lb (3 062 kg) when equipped with a canopy, full fuel tank and 24-inch (610-mm) bucket. The weight is down from the previous machine weight of 7,300 lb (3 311 kg), and this difference provides expanded margin to accommodate trailer weight and ancillary equipment while keeping total weight less than 10,000 lb (4 536 kg).
The new 303E CR is 60 inches (1550 mm) wide across the blade and has zero-radius tail swing. The machine is designed to work efficiently in small spaces and on congested job sites, and it’s easy to transport. The cab version will also benefit from the weight reduction.
For customers who do not need to meet the 10,000-lb (4 536-kg) transport requirement and wish to maintain the current machine weight, an optional 588-lb (267-kg) counterweight is available. This configuration is especially useful in heavy duty applications and when using heavy attachment configurations that include couplers and thumbs. The optimal counterweight brings the machine weight back to the current model weight of 7,300 lb (3 311) with a tail swing less than 5 inches (127 mm).
For more information about the Cat 303E CR, contact the local Cat dealer or go to: www.cat.com
Engine |
Cat C1.3 |
Net power, hp (kW) |
23.5 (17.5) |
Base Weight, canopy, lb (kg) |
6,750 (3,062) |
Extra Cwt -Weight, canopy, lb (kg) |
7,300 (3,311) |
Hyd. flow, gpm (L/min.) |
23.1 (87.6) |
Relief pressure, psi (bar) |
3,553 (245) |
Dig depth, max., in. (mm) |
108 (2,750) |
Dig height, max., in. (mm) |
178 (4,530) |
###
Note to Editors: Caterpillar rolls-out products and services in each of its territories at different time intervals. Although every effort is made to ensure that product information is released only after Caterpillar has received confirmation from our dealer network, our plants, and our marketing subsidiaries that products and services are available in the relevant region, editors are kindly requested to verify with their local dealer for product availability and specifications.
CAT, CATERPILLAR, their respective logos, “Caterpillar Yellow” and the “Power Edge” trade dress, as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.
©2017 Caterpillar All Rights Reserved
Press Inquiries |
Caterpillar Trade Press Media Representatives Americas Sharon Holling: Holling_Sharon_L@cat.com Johanna Kelly: Kelly_Johanna_L@cat.com Europe, Africa, Middle East Francine Shore: Shore_Francine_M@cat.com |
Reader Requests |
|
|