Hydrogen-Based Cat® Power Generation Solutions
Abstract
This paper provides an overview of hydrogen as a fuel source for on-site power generation and Caterpillar’s experience and plans for using hydrogen in reciprocating engines to power generator sets.
Introduction
This paper addresses the following questions:
- Why is there growing interest in hydrogen for energy production?
- When and how will hydrogen be widely available?
- What does hydrogen mean for reciprocating (recip) engines?
- What can Caterpillar offer in terms of on-site power generation with hydrogen?
WHY THE GROWING INTEREST?
Those involved with on-site power generation are becoming increasingly focused on decarbonization and greenhouse gas (GHG) reduction. Investors are looking beyond financial returns to evaluate companies and projects based on environmental, social, and corporate governance principles and progress. These trends show no signs of slowing and are creating a pull across industries and applications for power solutions that can help achieve GHG reduction goals.
For example, over the past 29 years (through 2019) the EU was able to achieve a GHG reduction of 24% which is 4% more reduction than the EU goal for 2020. In the next 10 years the goal is to reduce GHG by an additional 31%, compared to the actual reduction in 2019 and through 2050 the EU goal is to produce energy with zero GHG emissions. See Figure 1. This aggressive goal will require a rate of GHG reduction higher than has been achieved to date.
Beyond that, many countries have even more aggressive goals, with some aiming to be fossil fuel/carbon-free by 2045. Using hydrogen is one way to help meet these goals. Hydrogen burns carbon-free and can be produced from renewable resources. The production of renewable, or “green” hydrogen, also addresses the renewable energy supply/demand mismatch.
The graph in Figure 2 shows a typical view of the renewable energy supply/demand mismatch, which is significant and occurs on an hourly, daily, monthly, and seasonal basis. Supply and demand fluctuate by hundreds of terawatt hours, and an oversupply either necessitates the shutdown of renewable power plants or the storage of the surplus energy, both of which are costly and technically difficult.
To address this mismatch, Germany in 2020 spent approximately $1.5 billion to compensate renewable energy plants for shutdowns during periods of insufficient demand that resulted in oversupply.
Green hydrogen can help solve the demand/supply mismatch. Surplus renewable electricity can be used to produce green hydrogen that can then be used to fuel generator sets and provide the necessary load management needed for renewables. This also ensures that there is quality power in the grid during the deficits.
Despite the interest in renewable hydrogen as a fuel source to help achieve GHG reduction goals, there are challenges to its use as a replacement for diesel and/or natural gas – particularly in terms of power density and transient response. These and other important technical considerations are discussed later in this paper.
HYDROGEN AVAILABILITY
Hydrogen itself is colorless. The colors commonly assigned to hydrogen fuel – gray, brown, blue, pink, or green - describe the technology processes used to produce its different forms. The most widely discussed technologies are summarized in Figure 3.
Currently over 90% of hydrogen is made from natural gas (gray hydrogen) or coal (brown hydrogen). Gray hydrogen is produced by reforming natural gas. It is the lowest cost and most common form of hydrogen. Gray hydrogen provides no GHG reduction benefit.
When the fossil fuel process utilizes carbon capture technology to produce hydrogen it is called blue hydrogen.
Green hydrogen is produced through electrolysis from renewable electricity. It is expensive to produce relative to other forms of hydrogen due to the cost of production equipment and high transportation costs due to limited infrastructure for pure hydrogen. This is why we don’t see large quantities of green hydrogen on the market today. However, as the cost of electrolysis equipment reduces with scale and infrastructure is installed, costs for green hydrogen made from electrolysis will also drop similar to what we have seen with photovoltaics and batteries. Worldwide consumption of electricity is expected to double by 2050. With continued pressure for reduced-carbon energy sources to produce electricity, green hydrogen is expected to play an increasingly vital role in the world’s energy mix in the coming decades.
Caterpillar sees three pacesetters dictating the growth of hydrogen:
- Safety: Hydrogen is relatively easy to ignite and, being colorless and odorless, its presence can be difficult to detect.Hydrogen has been commonly used as feedstock and as a fuel source in certain applications for decades. As a result, significant experience and research have led to the establishment of protocols and standards for the safe storage, transport, anduse of hydrogen, which can be leveraged with increased hydrogen usage in the energy market with recip engines.
- Scale: As has been the case with photovoltaics, the increased production of hydrogen via electrolysis will result in economiesof scale to drive costs down.
- Supportive policy framework and investments: To significantly increase renewable hydrogen production, develop itsinfrastructure, further develop its power source technologies, and subsequently reduce its cost, there will need to be government and industry support. As an example, Germany will invest approximately $12 billion through 2025, including subsidies, to encourage the production of green hydrogen. In addition, many companies are taking steps and making investments toreduce their carbon footprint in order to meet their sustainability goals and are interested in green hydrogen as part of the future energy mix.
Pure hydrogen can be delivered directly to the consumer through a pipeline network, eliminating the need for storage, losses associated with transformation from gas to liquid and increased safety requirements with handling liquefied hydrogen. A pure hydrogen pipeline infrastructure could be accessed as easily as natural gas today, which would further stimulate utilization. Currently, the lack of infrastructure to deliver hydrogen is affecting its operating costs and economies of scale. To satisfy the anticipated demand for renewable hydrogen in Europe, there are plans for a hydrogen pipeline network which should be complete by 2030. There are already pure hydrogen pipelines operating within Europe, with plans to either build new pipelines or refurbish existing natural gas pipelines. The pipeline network may also be connected to the sun- and wind-rich areas of North Africa, where green hydrogen could be produced.
Caterpillar sees two distinct, but parallel paths in the ways hydrogen will be used in the future when hydrogen is plentiful:
- The blending of hydrogen with natural gas to create up to a 25% hydrogen mixture. This is attractive, as it makes use of the installed storage and distribution capacity. The concerns are mainly in the variability of blending, the proximity to blending locations, and limitations on household use since most boilers and other consumers of natural gas may need modifications towork with the higher levels of blended hydrogen.
- The use of 100% hydrogen or nearly 100% hydrogen at dedicated locations. This path will require specialized generatorsets and infrastructure.
As a result, Caterpillar sees the need for two different product classes: one using blends of up to 25%, and another enabling the use of 100% hydrogen.
HYDROGEN AS A FUEL FOR RECIP ENGINES
TECHNICAL CONSIDERATIONS
While the design of a hydrogen-enabled recip engine is similar to a standard natural gas engine, there are several factors to consider when accounting for the distinct properties of hydrogen. As shown in Figure 4 below, Caterpillar distinguishes these factors as follows:
- Green: Positive factors.
- Yellow: Factors to be considered but which can be managed.
- Red: Factors requiring significant modifications or with a safety concern.
The first of the positive (green) considerations for hydrogen is its wide range of flammability. This allows very lean fuel mixtures that combine with very low combustion temperatures to result in low NOx values. However, such low combustion temperatures may require a change in the engine’s cooling system.
The high diffusivity from hydrogen helps to form homogeneous mixtures and to create a well-mixed charge in-cylinder when utilizing port injection or direct injection fuel systems.
In considering manageable (yellow) factors, high laminar flame speed is positive because there is better efficiency out of the short combustion duration, but high pressure rise rates add mechanical stress to the engine. This increased mechanical stress can be managed through a combination of engine design and power derate. High auto ignition temperatures comparable to methane require no related changes.
Consideration must be given to the specifications for gas-carrying components to minimize the incidence of hydrogen leakage. To that end, one should adhere to suppliers’ application and installation instructions for items like proper engine room ventilation and proper hydrogen gas train installation.
Also, consideration must be given to material incompatibilities, specifically the steel embrittlement and O-ring deterioration caused by hydrogen. This requires careful analysis to ensure the correct materials are used in the engine.
Regarding the factors requiring significant modifications and/or safety concerns (red), low ignition energy increases the risk of knocking, pre-ignition, and backfiring, which drives the need for good engine control systems and management of the electrical systems per safety regulation requirements.
Small quenching distances drive the need for flame arrestors to have a much smaller mesh size in order to prevent combustion of the charge in the intake manifold which itself is a safety concern. The smaller mesh size requires higher air intake pressure, unless the size of the arrestors is increased. An alternative to fine mesh flame arrestors, used for hydrogen mixtures above 25%, to prevent pre-ignition in the intake manifold is port or direct injection of hydrogen.
Finally, the low density of hydrogen means there is less energy on a volume basis. A turbocharging system with a higher charge air pressure could be required to compensate for this factor and minimize the volumetric efficiency impact.
USER IMPACTS
The factors prioritized by many users of hydrogen include fuel source, power output, efficiency, emissions, capital and operating costs, and safety.
Different engine configurations can be optimized for power, efficiency, or hydrogen blending, but there are tradeoffs. This is illustrated by the performance of two hypothetical engines, as shown in Figure 5.
The blue oval represents a typical natural gas engine available on the market. This engine is able to operate with a hydrogen blend of up to approximately 25% without any significant derate. Thereafter, the engine derates until it can no longer run due to detonation, at which point the engine cannot accept additional load. However, efficiency is not affected, and in fact, it slightly increases when raising the hydrogen concentration from 0% to slightly under 25%.
The yellow oval represents an engine similar to those available on the market but with a decreased compression ratio, as well as minor changes to the software and the turbocharging system. This engine is able to operate with a hydrogen blend of up to 60% without any significant derate, and thereafter with a derate up to 100% hydrogen, where it is rated at approximately 60% of the natural gas rating. The electrical efficiency is lower than that of the production engine due to the lower compression ratio, but it stays more or less stable at 40%.
The GHG emissions of hydrogen steadily decrease to zero as the mixture goes to 100% hydrogen, as shown by the green line in Figure 6.The GHG and NOx reductionwith hydrogen blends isdetermined by the enginecombustion and controlssystems.
The blue dotted line shows an example of one engine configurations with a varying levels of blended hydrogen. For this engine, NOx emissions are unchanged up to about 20% hydrogen but thereafter the NOx emissions decrease. At 100% hydrogen, NOx emissions are approximately 10% of the initial value and there are virtually no GHG emissions. Also, there are no unburned hydrocarbons, which means an oxidation catalyst is not needed.
This results in a win- win situation, with very low initial cost and clean exhaust gas. The concept of low emissions and capital costs has been demonstrated in data center applications with 3 MW generator sets, which is a typical rating node for this application. User installed costs for different technologies are shown in Figure 7.
The initial costs of diesel engines are relatively small, and they increase when looking at natural gas engines because of the lower power density. Initial costs increase again with hydrogen engines. In all cases, the cost of a generator set is still not high when compared with current fuel cells and batteries. Though the costs for fuel cells and/or batteries may fall in the future.
Additional costs are shown in blue for aftertreatment systems, while energy storage systems are shown in gray. Energy storage is a technology which can be utilized in conjunction with recip engines, turbines, and fuel cells to achieve transient performance requirements, but it does add costs.
Finally, the salmon bars represent a relatively larger portion of the infrastructure cost for liquefied hydrogen tanks, which can raise the initial cost of a recip engine generator set using hydrogen to approximately three times that of a recip generator set using diesel fuel.
A different picture emerges when considering operating costs, as shown in Figure 8. Operation with natural gas is less costly than diesel since it is a less expensive fuel. When considering hydrogen produced from natural gas (gray hydrogen), the costs for the fuel itself are still below that of diesel. However, two additional bars represent costs to liquify or compress hydrogen and then transport it.
When considering hydrogen produced from renewables (green hydrogen), the additional costs for infrastructure are the same, but the production costs are expected to be five times higher than those for gray hydrogen through the 2025 timeframe. This highlights the need for supportive policy framework and investments in green hydrogen infrastructure to reduce production costs and make green hydrogen commercially viable.
The production costs of renewable hydrogen are eventually expected to be reduced and could match natural gas or diesel.
With respect to safety, hydrogen is odorless, tasteless, and colorless, and current odorants are not light enough to travel with hydrogen. As a result, readily available sensors are needed at all times to detect hydrogen concentrations.
Figure 9 shows photos of propane flames next to hydrogen flames and prove the difficulty in visually detecting hydrogen flames. The propane flame is highly visible in daylight, while the hydrogen flame is nearly invisible. Using an infrared filter, the propane flame is highly visible, while the hydrogen flame is barely visible.
CATERPILLAR’S OFFERING FOR HYDROGEN
Caterpillar has experience using a wide range of alternative fuels in its gas generator sets. This includes hundreds of thousands of operating hours using hydrogen fuel mixtures.
Caterpillar views green hydrogen as one of the fuel sources that can contribute to a reduced-carbon future. It is currently testing or has plans to test higher hydrogen mixtures and 100% hydrogen on single-cylinder engines at Caterpillar facilities and multi-cylinder engines at Caterpillar facilities and customer sites. This work leverages Caterpillar’s deep performance simulation experience, especially on combustion and flame propagation.
In addition, work is underway on projects funded by grants from the U.S. Department of Energy’s Office of Energy Efficiency and Renewable Energy (EERE) and the German Federal Ministry for Economic Affairs and Energy (BMWi). The EERE project involves a 2.0 MW combined heat and power (CHP) system and will demonstrate flex-fuel operation on 100% hydrogen as well as various blends of hydrogen and natural gas. The BMWi project will involve a 400 ekW generator set running on various mixtures of up to 100% hydrogen to better understand load and efficiency optimization.
The experience and development work referenced above will allow the commercial launch of solutions for Cat gas gensets rated 400 – 4,500 ekW to operate on up to 25% hydrogen blends by the end of 2021. This will be concurrent with the commercial launch of the G3516H generator set at a rating of 1,250 ekW configured for 100% hydrogen.
CONCLUSION
Hydrogen, specifically green hydrogen, is one of the fuels being considered to help to reduce the carbon footprint of those involved in on-site power generation using recip engines.
There are a number of factors influencing mass adoption of hydrogen as a fuel source. Some of these factors should see positive movement in the coming years.
While there are a number of tradeoffs and factors to consider in burning hydrogen in recip engines, hydrogen can add value for on-site power generation applications.
Caterpillar is already offering recip engines (and turbines) capable of operating on hydrogen and hydrogen blends. We continue to improve the capability of hydrogen-powered reciprocating engines with minimal impact on maintenance costs and schedules, availability, and operations. We are continuing to invest in hydrogen technology and are well positioned to serve the needs of power generation customers and the marketplace as green hydrogen becomes more readily available.