If you already have an existing account with another Cat App, you can use the same account to sign in here
One Account. All of Cat.
Your Caterpillar account is the single account you use to log in to select services and applications we offer. Shop for parts and machines online, manage your fleet, go mobile, and more.
Account Information
Site Settings
Security
Efficient power solution can deliver up to $250,000 in fuel savings for offshore supply vessels
Hamburg, Germany - Caterpillar Marine is pleased to announce the launch of the Mak M 25 E engine platform at the 2014 SMM Exhibition, held September 9 -12 in Hamburg, Germany. Developed for state-of-the-art vessel designs with an emphasis on fuel savings, the platform was specifically designed to address the evolving global marine industry requirements while maximizing operators’ bottom line. Key product features include optimized engine performance as well as an efficient part load range, which can help to save up to 40 tons of fuel a year when operating vessels at variable engine speed. Vessels typically operating at lower loads can save up to 60 tons of fuel per year by changing the operating mode from constant- to variable engine speed. The M 25 E will be available to order from the global MaK dealer network in fourth quarter 2014 and is ideal for offshore and coastal cargo vessels.
Caterpillar Marine senior product definition engineer Detlef Kirste commented, “The reliability of the new MaK 25 E is assured, given that it is based on the legendary M 25 C platform. In addition to adding a 5 percent power increase and reducing the fuel consumption on this platform, we also engineered the M 25 E to capitalize on the synergies between the engine, vessel and propulsion system.”
Developed to be compatible with both traditional and modern mechanical systems as well as electric propulsion systems, the M 25 E will be available in 6, 8 and 9 cylinder configurations offering ratings between 2,100 kW and 3,150 kW at 720 and 750 rpm.
By combining a set of proven technologies such as Flexible Camshaft, Waste Gate Technology and Cylinder Bypass Valve, Caterpillar Marine engineers designed engine ratings to support varied operational profiles of vessels at lowest smoke emissions while supporting the installation of Selective Catalytic Reduction (SCR) systems for lowest NOx emissions at the same time.
The engine is ideal for vessels where the hull and propeller have been optimized for lowest operational costs at cruising speeds as well as for vessels where customers have elected to lower operational fuel costs by utilizing selected load profiles in combination with the most efficient engine speed. Equipped with the new Modular Alarm and Control System (MACS) the M 25 E also supports remote condition monitoring and diagnostic maintenance programs.
The customizable M 25 E was designed to leverage Cat Propulsion solutions and is available in controllable pitch and fixed pitch propeller applications as well as generator applications.
“The M 25 E has a very high torque to speed ratio allowing operators to run their CP propellers at a reduced propeller shaft speed significantly increasing the propulsive efficiency and lowering fuel consumption,” Jonas Nyberg Caterpillar Propulsion sales manager noted. “The improved load response also makes them the ideal engines for any demanding transient operations such as Dynamic Positioning."
Cat® marine power and propulsion solutions are backed by the worldwide Cat dealer network with trained technicians to ensure service support is never out of reach. Visit us at SMM Hamburg in Hall A4 at Booth #204. For more information on Caterpillar Marine, visit www.marine.cat.com. For information on Cat Propulsion products, visit www.catpropulsion.com. Follow us on Facebook: www.facebook.com/caterpillarmarine and Twitter @catmarineglobal.
# # #
Caterpillar Marine, with headquarters in Hamburg, Germany, groups all the marketing and service activities for Cat and MaK™ marine diesel, dual fuel and gas power and propulsion systems within Caterpillar Inc. The organisation provides premier power solutions in the medium- and high-speed segments with outputs from 93 to 16,800 kW in main propulsion and 10 to 16,100 kWe in marine generator sets as well as a comprehensive portfolio of propulsion solutions. The sales and service network includes more than 2,100 dealer locations world-wide dedicated to support customers in ocean-going, commercial marine and pleasure craft wherever they are.
More information is available at: MARINE.CAT.COM/pr
For nearly 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2013 sales and revenues of $55.656 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Resource Industries, Construction Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.
Press Inquiries
Jenna Janik Marcoux
Phone: +1 713 895 1449
Marcoux_Jenna_J@cat.com